Arduino Forum Radio Control Help Please (Arduino)
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
  • State Verified Answer
  • Replies 11 replies
  • Answers 4 answers
  • Subscribers 405 subscribers
  • Views 1120 views
  • Users 0 members are here
Related

Radio Control Help Please (Arduino)

hank_the_electric_explorer
hank_the_electric_explorer over 8 years ago

     I am trying to upgrade a  my robot I built. I Have a IR remote control which has about a ten-twenty foot range. I am buying a new chassis and everything but I am having trouble understanding the basics of Radio control. I have googled "Arduino RC", but it is way to complicated for me. I understand the basics of Arduino coding and the bare bones of remote control but it gets a bit complicated.

 

My Questions are : Is their a easy trick I can learn with the Arduino to help get a radio controlled robot? ( Like in this tutorial with pressing a button and putting the numbers in the code)

     Is their a tutorial some where that explains a lot about Radio control that is easy and no complicated?

     (Any other suggestions for radio control)

 

 

                       

                         Any help is appreciated!

                                                                 Thanks!        

                                                                           Ben     

                              

       

  • Sign in to reply
  • Cancel

Top Replies

  • COMPACT
    COMPACT over 8 years ago +1 suggested
    IR control is Radio control using the Infrared wavelengths. Adapting to other forms is easy if you understand how the IR control works. Using other wavelengths may entail different encoding methods better…
  • vandia
    vandia over 8 years ago +1 verified
    Hi Ben! First, since it's not clear from your post, I wanted to make absolutely sure you know there's a difference between radio (RF) and infrared (IR). -IR typically has wider ranger and has a much lower…
Parents
  • WarrenW
    0 WarrenW over 8 years ago

    Essentially the Radio link can easily be setup, the structure of the data can be preset to an array of data bits and these bits can be used by the receiver to turn on/off the controls. Pretty simple for on/off control.

    Now if there is a need to get a proportional system running, e.g. steering via a pot or speed control you will need to transmit a little bit more in the way of a complex signal as the analogue value of your input will need to be transferred. Again that can be handled in the structure of the data that you define and the analogue signal could then be extracted and used to drive a PWM servo system of sorts.

     

    Great to see another member exploring the Arduino platform.

    I am still getting to grips with mine.

     

    Cheers

    Warren.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • WarrenW
    0 WarrenW over 8 years ago

    Essentially the Radio link can easily be setup, the structure of the data can be preset to an array of data bits and these bits can be used by the receiver to turn on/off the controls. Pretty simple for on/off control.

    Now if there is a need to get a proportional system running, e.g. steering via a pot or speed control you will need to transmit a little bit more in the way of a complex signal as the analogue value of your input will need to be transferred. Again that can be handled in the structure of the data that you define and the analogue signal could then be extracted and used to drive a PWM servo system of sorts.

     

    Great to see another member exploring the Arduino platform.

    I am still getting to grips with mine.

     

    Cheers

    Warren.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer