Arduino Forum What kind of sensor can I use to determine approximate distance of small animal?
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
  • State Suggested Answer
  • Replies 19 replies
  • Answers 9 answers
  • Subscribers 396 subscribers
  • Views 1285 views
  • Users 0 members are here
Related

What kind of sensor can I use to determine approximate distance of small animal?

nosrol
nosrol over 8 years ago

I am using an Arduino Uno and it will be in an inside environment. I want to determine if the arduino is getting closer or farther from a pet. I have been playing around with the idea of either a Microwave Doppler Radar, however, that is more for movement than distance. IR sensors won't detect through walls, plus the pets are black and absorb much of the radiaiton. Ultrasonic is out of the question as it disturbs the pets. Any other ideas or maybe something I am overlooking?

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 8 years ago +2 suggested
    Use the Grid Eye sensor. It can detect small IR signatures up to about 5 meters. DAB
  • COMPACT
    COMPACT over 8 years ago in reply to nosrol +2 suggested
    Use more cameras - on each side of the wall. Use RF to communicate to the cameras.
  • djfraz
    djfraz over 8 years ago +2 suggested
    Have you considered an iBeacon. Most mobile apps can give you a distance measurement once calibrated. It can be done using an intel edison, i think it can be done on the esp32 module as well
Parents
  • wmbell65
    0 wmbell65 over 8 years ago

    i think the technology will depend on additional parameters.. is this strictly indoors or outside as well? What distances are you looking to detect at? Are you looking to track the animal or react when it gets close?

    you could look at a variation of geo fencing using rfid tags and antennae in various rooms.. if you are looking at a reactive system, motion sensors and proximity sensors might do the trick

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • wmbell65
    0 wmbell65 over 8 years ago

    i think the technology will depend on additional parameters.. is this strictly indoors or outside as well? What distances are you looking to detect at? Are you looking to track the animal or react when it gets close?

    you could look at a variation of geo fencing using rfid tags and antennae in various rooms.. if you are looking at a reactive system, motion sensors and proximity sensors might do the trick

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer