Arduino Forum Read data input from shift register
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
  • State Suggested Answer
  • Replies 19 replies
  • Answers 3 answers
  • Subscribers 393 subscribers
  • Views 2303 views
  • Users 0 members are here
  • shift register
  • multiplexing
  • frontpage
Related

Read data input from shift register

tim687
tim687 over 8 years ago

I am having some troubles getting the readouts from the shift register.

The 74HC_HCT164 controls a EADCD040YA2 (or alike) two digit 7 segment display.

Is there any way that I could reliably read the Serial input data from the shift register.

 

I have got a pin-out of the shift register to the display, so that shouldn't be any problem.

 

What might be useful to know, is that the shift register circuit is not only used for the display, but also for some of the LED's.

The data is shifted into the shift register, then the first common anode is turned on by the microprocessor, then the shiftregister latches, shift register clears, second diigit data get's shifted in, second common anode is turned on, shift register latches and shift register clears.

 

I don't know if there is happening anything between the two digit 'shift's' and what's the clock cycle of the whole circuit. I don't have access to an ocsilloscope, well, I do if you call my Arduino one.

 

I am using an Arduino to read out the code (using the following sketch: https://pastebin.com/8fWA6qUP)

 

I would appriciate it very much if anyone could help me out with this problem!

 

So to be clear: this is NOT about using a shift register the normal way, but to basically hack shift register and read what's being send to it!

 

Tim

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +1 suggested
    tim687 The 74HCT164 is a serial to parallel converter. Basically you set the state you want on that particular output using the two inputs and then raise the clock. You need to do this 8 times to replace…
  • mcb1
    mcb1 over 8 years ago in reply to tim687 +1 suggested
    Is this related to this. Detect whether a pin is connected to GND I posted a link where a local person has been able to detect the serial output from an Aircon unit. https://nicegear.co.nz/blog/hacking…
Parents
  • mcb1
    0 mcb1 over 8 years ago

    tim687

    The 74HCT164 is a serial to parallel converter.

    Basically you set the state you want on that particular output using the two inputs and then raise the clock.

    You need to do this 8 times to replace/set all 8 outputs

    image

     

    You need to read the value of the two data lines, and note them when the clock goes high.

    You'll also need to check if the MR line is able to change, since it will reset the outputs.

     

    Most 7 segment displays only need 4 bits, which means they could easily use the other 4 outputs for something else.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tim687
    0 tim687 over 8 years ago in reply to mcb1

    So you'd say I'd have to read out input A and B from the shift register and perform a (bit wise) AND operation onto them to get the input data?

     

    The problem I'm having is that the two (serial coded) digits sometimes get swapped around.

     

    The display definitely is a 8 bit display. It has got a total of 10 pins, 2 common anodes and 8 data pins.

     

    The problem is however, that I will be using this in an IoT project, so I'm starting to get very tight with the available pins. I've freed up two pins using, how hilarious image, a shift register.

    That means that I only have a pin for the serial input A and the clock. I could free up more pins by using a shift in register, but I think that it would make the whole project to complex than it needs to be.

     

    Thanks for your diagram though! I haven't searched for one to be honest image

     

    Thanks again!

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 8 years ago in reply to mcb1

    According to the datasheet of the micro, the chip doesn't have any SCI (Serial Communication Interface)

     

    Besided checking both inputs, any other options?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago in reply to tim687

    Probably supposed to say SPI, not SCI ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 8 years ago in reply to Robert Peter Oakes

    Nope, the chip doesn't have SCI (serial/UART) and SPI according to my research.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to tim687

    Besided checking both inputs, any other options

    Not really.

    If this is the same circuit as you gave in the other link, then there is a single Input data line, and a clock.

    There must be a second select line for the digits.

     

     

    A Parallel to Serial will simply give you back the input data, and you still need to read it.

    Googling Binary to BCD gives lots of hits but nothing really sticks out.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 8 years ago in reply to mcb1

    The schematic isn't fully complete, but for a parallel to serial chip, how do I deal with the two digits being send? Do I need to connect the clock signals from the original register to the parallel to serial one?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to tim687

    Do I need to connect the clock signals from the original register to the parallel to serial one

    Yes and there is the issue.

    You actually don't really save anything in terms of pin numbers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 8 years ago in reply to mcb1


    I do if I use the inverse of a shiftregister (shift in register), right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to tim687

    I don't think you'll ever pull this off without a scope or  a logic analyzer.

     

    A scope may well be outside your budget but you may be able to afford a cheap logic analyzer.

     

    hobby components usb 8ch 24mhz 8 channel logic analyser. compatible with saleae software.

     

    This one is typical of the cheapest - it's limited to 24MHz which might be a problem (the clock to the shift register might be faster than this). I haven't used it so it may be rubbish - look for reviews.

     

    To sort out how the display drive is working you need  to monitor the clock, data and anode signals - so you need at least 4 channels - once you know the protocol you may be able to decode what is sent with less.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to michaelkellett

    you need  to monitor the clock, data and anode signals - so you need at least 4 channels

    If the circuit is the same as the link the two data inputs are paralleled, so 3 channels, but yes otherwise I agree a logic probe or scope is required.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 8 years ago in reply to tim687

    Tim Koers wrote:

     

    I've created a little schematic, the output pins of the shiftregister Q0-Q7 (in order) corresponds to the pins A-G and DP.

    I've also figured out which pin controls which segment, but the strange thing is that there is no correlation between the serial input and the expected serial input according to my pin to segment research.

     

    I got it working at some point, but only for a few numbers. (17, 21, 23, 25, 26, 27)

     

    Is there something I might be missing?

    Can you have a look and see what the part number of Q1 and Q2 is?

     

    Most likely the circuit is something like this, with Q1 and Q2 being PNP transistors:

     

    image

     

    The 7-seg display is in two halves. The display of one digit is done first, then the other. The transistors enable whichever display is the right one for the data that has just been loaded into the shift register. If I'm right with the circuit, the processor will normally hold all the base drives high and take just one of them low to enable.

     

    The circuit is actually even more complicated, because the separate LEDs are driven the same way as the 7-segment LEDs and will have their turn too, probably enabled with Q3 or Q4.

     

    To disentangle this with an Arduino, you'd need to be reading the 4 lines of the multiplex drive so that you knew which data you were getting from the s/r.

     

    This is much easier with a scope because you can see the drive waveforms, see the order they go in, and see how much time you get to read the data.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 8 years ago in reply to tim687

    Tim Koers wrote:

     

    I've created a little schematic, the output pins of the shiftregister Q0-Q7 (in order) corresponds to the pins A-G and DP.

    I've also figured out which pin controls which segment, but the strange thing is that there is no correlation between the serial input and the expected serial input according to my pin to segment research.

     

    I got it working at some point, but only for a few numbers. (17, 21, 23, 25, 26, 27)

     

    Is there something I might be missing?

    Can you have a look and see what the part number of Q1 and Q2 is?

     

    Most likely the circuit is something like this, with Q1 and Q2 being PNP transistors:

     

    image

     

    The 7-seg display is in two halves. The display of one digit is done first, then the other. The transistors enable whichever display is the right one for the data that has just been loaded into the shift register. If I'm right with the circuit, the processor will normally hold all the base drives high and take just one of them low to enable.

     

    The circuit is actually even more complicated, because the separate LEDs are driven the same way as the 7-segment LEDs and will have their turn too, probably enabled with Q3 or Q4.

     

    To disentangle this with an Arduino, you'd need to be reading the 4 lines of the multiplex drive so that you knew which data you were getting from the s/r.

     

    This is much easier with a scope because you can see the drive waveforms, see the order they go in, and see how much time you get to read the data.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tim687
    0 tim687 over 8 years ago in reply to jc2048

    There aren't any transistors connected to the s/r. The enable lines of the I individual segments is controlled trough a transistor that is connected to the main microcontroller.

     

    I'll have to check if I can get my hands on a scope I think.

     

    I am always open for suggestions about a good scope.

     

     

    Regarding Q0 till Q7, those are the outputs of the s/r