Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Imported Arduino Project Not Working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 8 answers
  • Subscribers 416 subscribers
  • Views 1995 views
  • Users 0 members are here
  • energia
  • tiva c
  • grideye
  • msp430
  • arduino
Related

Imported Arduino Project Not Working

kas.lewis
kas.lewis over 9 years ago

Hello,

 

I am attempting to run an Arduino project on on of my TI boards. I have a Maxim 1-Wire demo board that uses an Arduino for as its platform, not having one I decided to try a TI board. I load the required Libraries but I get an interesting issue. Even though there are two OneWire and I point it to the one I want to use it only finds some header files and not others. I have tried pointing to teh needed files with exact paths with no luck. To be sure I tried complaining teh same project in the Arduino IDE and there are no issues at all, include the needed libraries and it compiles. If someone could help explain what I am missing and why it finds some library files and not others that would be great.

 

Thanks

Kas

 

I know this is a repost but as I was unsure where to post it I have reposted it, If you could clarify the correct place I would be more than happy to remove any duplicate posts.

 

C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -dump-prefs -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_976722\MAXREFDES131_GUI_Firmware.ino"
C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -compile -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_976722\MAXREFDES131_GUI_Firmware.ino"
Using board 'MSP-EXP430F5529LP' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
Using core 'msp430' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
Detecting libraries used...
"C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
"C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
Generating function prototypes...
"C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\preproc\ctags_target_for_gcc_minus_e.cpp"
In file included from C:\Users\Kas\Documents\Energia\libraries\OneWire-master\src\OneWire.h:37:0,

                 from C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_976722\MAXREFDES131_GUI_Firmware.ino:40:

C:\Users\Kas\Documents\Energia\libraries\OneWire-master\src\/Masters/Masters.h:38:42: fatal error: Masters/DS248x/DS2484/DS2484.h: No such file or directory

compilation terminated.

exit status 1
Error compiling for board  MSP-EXP430F5529LPMSP-EXP430F5529LP

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +3 suggested
    Hi Kas, I reckon possibly what's going on is that the path should be DS248x/... in the #include if the #include is using double-quotes, otherwise it is expecting the folder path to have two 'Masters' folders…
  • balearicdynamics
    balearicdynamics over 9 years ago +1 suggested
    Hello Kas, I have used in past (and already I have it installed on my computer) both energia (developed by TI from the original Arduino IDE) and the original Arduino IDE. Please edit your post and set…
  • rsc
    rsc over 9 years ago +1 suggested
    There's a typo in this line "master\src\/Masters/Masters.h:38:42: fatal error:" look at "src\/" Scott
Parents
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Hello Kas,

     

    I have used in past (and already I have it installed on my computer) both energia (developed by TI from the original Arduino IDE) and the original Arduino IDE. Please edit your post and set the report with Syntax highlighting / Plain to make it more readable else it is almost impossible to see what happens.

    You find this features in the post edit menu as shown in the image below.

     

    Thank you. Enrico

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Hello Kas,

     

    I have used in past (and already I have it installed on my computer) both energia (developed by TI from the original Arduino IDE) and the original Arduino IDE. Please edit your post and set the report with Syntax highlighting / Plain to make it more readable else it is almost impossible to see what happens.

    You find this features in the post edit menu as shown in the image below.

     

    Thank you. Enrico

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • kas.lewis
    0 kas.lewis over 9 years ago in reply to balearicdynamics

    Hello Enrico,

     

    I would agree that the syntax highlighting helps, unfortunately in this case it's just output text from the "debugger" there is no code there at all. Thank you for the suggestion though.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to kas.lewis

    Hello Kas,

     

    thank you for the answer. When there is just a compilation output or similar, you can use the syntax highlighting "plan" mode. This helps a lot showing text as it is send to the terminal output. Now I have just copied and pasted your text below. The result is not 100% satisfactory as probably the E14 edito has already done its job with CSS but if you copy and paste as plain formatting I think you can get better results. It's not an option as I found very difficult to read your output.

     

    Enrico

     

    C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -dump-prefs -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_976722\MAXREFDES131_GUI_Firmware.ino"
    C:\Users\Kas\Desktop\energia-1.6.10E18\arduino-builder -compile -logger=machine -hardware "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware" -hardware "C:\Users\Kas\AppData\Local\Energia15\packages" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\tools-builder" -tools "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430" -tools "C:\Users\Kas\AppData\Local\Energia15\packages" -built-in-libraries "C:\Users\Kas\Desktop\energia-1.6.10E18\libraries" -libraries "C:\Users\Kas\Documents\Energia\libraries" -fqbn=energia:msp430:MSP-EXP430F5529LP -ide-version=10610 -build-path "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp" -warnings=default -prefs=build.warn_data_percentage=75 -verbose "C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_976722\MAXREFDES131_GUI_Firmware.ino"
    Using board 'MSP-EXP430F5529LP' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
    Using core 'msp430' from platform in folder: C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430
    Detecting libraries used...
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "nul"
    Generating function prototypes...
    "C:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/bin/msp430-g++" -c -g -O2  -w -fno-exceptions -ffunction-sections -fdata-sections -fno-threadsafe-statics  -w -x c++ -E -CC -mmcu=msp430f5529 -DF_CPU=16000000L -DARDUINO=10610 -DENERGIA=10610 -DENERGIA_MSP-EXP430F5529LP -DENERGIA_ARCH_MSP430 -IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\tools\msp430/include  "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\cores\msp430" "-IC:\Users\Kas\Desktop\energia-1.6.10E18\hardware\energia\msp430\variants\MSP-EXP430F5529LP" "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\sketch\MAXREFDES131_GUI_Firmware.ino.cpp" -o "C:\Users\Kas\AppData\Local\Temp\builda12a5302e2fbcba7b0882b591878e19b.tmp\preproc\ctags_target_for_gcc_minus_e.cpp"
    In file included from C:\Users\Kas\Documents\Energia\libraries\OneWire-master\src\OneWire.h:37:0,
                     from C:\Users\Kas\AppData\Local\Temp\arduino_modified_sketch_976722\MAXREFDES131_GUI_Firmware.ino:40:
    C:\Users\Kas\Documents\Energia\libraries\OneWire-master\src\/Masters/Masters.h:38:42: fatal error: Masters/DS248x/DS2484/DS2484.h: No such file or directory
    compilation terminated.
    exit status 1
    Error compiling for board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer