Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Uno circuit fault finding
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 4 answers
  • Subscribers 416 subscribers
  • Views 2323 views
  • Users 0 members are here
  • lcd
  • keypad
  • digital code lock
  • uno
  • newbie
  • question
Related

Uno circuit fault finding

Fevvahz
Fevvahz over 9 years ago

Hi, i'm new to Arduino, and I'm having a few issues with my first project.  I decided to try and recreate the Digital Code Lock project posted on Digital Digest.  I'm struggling with configuring the circuit itself.

 

I've successfully uploaded the code to the Uno, but there's a few issues;

 

-the buzzer sounds constantly.

- the LCD display doesn't power up

 

I've tried to lay the circuit out in a way that's straightforward to follow, but as I say, i'm pretty new to this.  I found the circuit diagram hard to follow, as some of the connections shown differed slightly with my hardware (I tried to get as close to what the original poster listed as possible), especially the keypad.  I suspect I've connected it up wrong, or put a component the wrong way round.  I've dont some fault finding with my multi meter, and power seems to be getting to the components.

 

I've attached some images.  Can anyone tell me firstly if it looks like I've connected it up wrong?

 

Message was edited by: Chris Swann - pictures added.

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago +4 suggested
    Fevvahz wrote: -the buzzer sounds constantly. It looks from the pictures that you may have 3.3V permanently applied over the buzzer. If you follow the connection of the 3V3 and GND signals from the Arduino…
  • Fevvahz
    Fevvahz over 9 years ago +3 suggested
    Well the beer flowed, and was welcome. Now, its time to conclude my tale.... Firstly, I had the jumpers from outputs 8,9,10 and 11 on the Arduino to the pins 12, 13, 14 and 15 respectively, instead of…
  • gadget.iom
    gadget.iom over 9 years ago +2 suggested
    Hello Fevvahz I cannot see the images you attached. If you could post them on here I'll take a look at the circuit for you. Paul
Parents
  • gadget.iom
    0 gadget.iom over 9 years ago

    Hello Fevvahz

     

    I cannot see the images you attached. If you could post them on here I'll take a look at the circuit for you. image

     

    Paul

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 9 years ago

    Hello Fevvahz

     

    I cannot see the images you attached. If you could post them on here I'll take a look at the circuit for you. image

     

    Paul

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Fevvahz
    0 Fevvahz over 9 years ago in reply to gadget.iom

    Paul - sorry about that - I added them as attachments, but I'll post them inline instead;

    HOvimn8.jpg

     

    Yi209Lg.jpg

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 9 years ago in reply to Fevvahz

    Hi Fevvahz

     

    I'd go back over your wiring for the transistor/buzzer section of the circuit. The schematic shows the base of the transistor being connected to pin A1 of the Arduino through a resistor. I cannot see that connection on your photos, nor can I see a resistor.

     

    As rachaelp has already pointed out, the buzzer seems to be permanently wired to the 3.3V supply, completely bypassing the transistors. And as she also stated, you probably aren't getting a suitable connection from the glue on the LCD header.

     

    Also check the configuration of the wiring around the resistor for your LCD. It looks like you might have interpreted a join at the resistor/VEE junction which is actually not connected to VDD (No dot).

     

    Take a look at these suggestions and get back to us with your findings. image

     

    Paul

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Fevvahz
    0 Fevvahz over 9 years ago in reply to gadget.iom

    Paul - thanks for your reply.  I did wonder about that resistor, it shows a 220 ohm on the diagram doesn't it?  I'll take another look at it and see how I get on once I've soldered on some 0.1 headers to the LCD screen.  Thanks again!