Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Using 40 low frequency Mics.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 12 answers
  • Subscribers 418 subscribers
  • Views 3777 views
  • Users 0 members are here
Related

Using 40 low frequency Mics.

noblemaster
noblemaster over 9 years ago

Hi,

I am working on a device that takes input from 40 microphones and send data to PC via Arduino.

I want to use low frequency microphones (5Hz onwards) with around 200-250Hz sampling for each mic.

 

For this purpose, my preliminary design is like this...

    40 Mics --> 40 PreAmp circuits --> Mux Shield II --> Arduino DUE --> PC

 

Please suggest me suitable commercial available preAmp circuits and any suggestion on the design is most welcome.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago in reply to noblemaster +2 suggested
    Your answer suggests you are willing to spend over $1000 per channel to get the best possible. If that is not true, the description needs to be more complete in order to get a helpful answer.
  • michaelkellett
    michaelkellett over 9 years ago in reply to noblemaster +2 suggested
    To measure at up to 100Hz you need to sample each microphone at 500Hz or faster. For each microphone you will need a a buffer amplifier as shown on the Invensys data sheet and an anti-aliasing low pass…
  • rachaelp
    rachaelp over 9 years ago in reply to DAB +2 suggested
    DAB is right, the USB on the Arduino is serial over USB, i.e. it just shows up as a serial port on the PC and you'll probably be maxed out at 115200 baud (I may be wrong here but you should look into it…
Parents
  • rachaelp
    0 rachaelp over 9 years ago

    Most commercial mic pre circuits I believe have DC blocking caps so they are suitable for use with phantom powered mics. As such they have an inherent roll off at low frequencies so you'll be struggling to get a decent level through most sensibly priced ones at 5Hz. There are some exceedingly expensive options such as http://www.studiocare.com/summit-ecs-410-everest-channel-strip.html which are fairly flat down to 5Hz but for your 40 mics it'll set you back nearly £30k..... Given that your design uses an Arduino, I am thinking this is not the price budget you're aiming at....

     

    I think you might be better off designing your own 40-input mic preamp (or a single one 40 times or something in between) which work for your specific requirements. Speaking of which, if you could expand on those with more details (i.e. a little more than "As much as possible") and maybe give some background for your specific application then people might be able to help you more easily.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • noblemaster
    0 noblemaster over 9 years ago in reply to rachaelp

    I am interested in measuring vibrations in 5Hz to 100Hz band and then analysis in MATLAB.. Mic model ICS40300. Signal is good with DC offset at 0.8V and max output at around 1.2V.

    I am using Arduino DUE, it has 12 bit ADC. I have few options in mind...

     

    1. https://www.sparkfun.com/products/9816

    What if I change its input cap at both stages from 1uF to 4.7uF?

     

    2. https://www.sparkfun.com/products/9868

    What if I replace its microphone with my desired model and change its input cap to 27uF?

     

    Which option is better from above two? or something else is required?

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • WarrenW
    0 WarrenW over 9 years ago in reply to noblemaster

    Hi Noble.

    When calculating the low frequency cut off 3dB point you can do some simple maths of 1/(2 x Pi x Freq x Capacitor) to give the reactance and given the 10Kohm input on the 9816 module your reactance would need to be the same for a simple -3dB point (1/2 the amplitude). It's a simple voltage divider at that point.

    The 1uF gives about 33Kohm at 5hz.

    A 4.7uF would be approx. 6Kohm so should be able to amplify you 5 Hz with 'some' reduction in amplitude from the original waveform. DAB suggested superimposing a 1Khz 'carrier' and then filtering this which is a logical solution if you are going to MUX the inputs as the MUX rate will alter you LF waveforms.

     

    Now we take the MIC into account - whoa - it has a 3dB point of 6Hz! That will mean your levels will already be skewed. I hope you are not looking to analyse on amplitude and hope you are analysing freq only (i.e. presence of frequency not how loud).

     

    After about 10Hz things should flatten off.

    Hope this helps.

    Warren.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • WarrenW
    0 WarrenW over 9 years ago in reply to noblemaster

    Hi Noble.

    When calculating the low frequency cut off 3dB point you can do some simple maths of 1/(2 x Pi x Freq x Capacitor) to give the reactance and given the 10Kohm input on the 9816 module your reactance would need to be the same for a simple -3dB point (1/2 the amplitude). It's a simple voltage divider at that point.

    The 1uF gives about 33Kohm at 5hz.

    A 4.7uF would be approx. 6Kohm so should be able to amplify you 5 Hz with 'some' reduction in amplitude from the original waveform. DAB suggested superimposing a 1Khz 'carrier' and then filtering this which is a logical solution if you are going to MUX the inputs as the MUX rate will alter you LF waveforms.

     

    Now we take the MIC into account - whoa - it has a 3dB point of 6Hz! That will mean your levels will already be skewed. I hope you are not looking to analyse on amplitude and hope you are analysing freq only (i.e. presence of frequency not how loud).

     

    After about 10Hz things should flatten off.

    Hope this helps.

    Warren.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer