Arduino Forum Is this crap or acceptable work ?
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
  • State Verified Answer
  • Replies 13 replies
  • Answers 9 answers
  • Subscribers 394 subscribers
  • Views 1046 views
  • Users 0 members are here
  • solder
  • diy
  • arduino
Related

Is this crap or acceptable work ?

neliger
neliger over 8 years ago

Hi to the community image

 

There is a long time since my last solder work. I've made a little thing today that looks like a wanted on the front, but (I think) looks like crap on the back lol

 

I would love to hear from all DIY lovers about this work : does it looks like I'll go to the electronic hell for having done this, or is this way to do it acceptable ?

 

For the record, this will be worn with a string around the neck, as it, just with some kapton on the back to protect cables.

 

Other question : is it insane to wear for a day an unprotected LiPo like this ?

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 8 years ago +6 verified
    Hi Loic, In general, I think you are using too much solder. Remember, the goal is to bond the wire or lead to the pad. You first want to make sure you have a good physical connection by crimping the wire…
  • shabaz
    shabaz over 8 years ago +6 suggested
    I agree with all the comments so far. Some things could be tweaked (like amount of solder, amount of heat, maybe even the component leads could be heavily oxidised if they are from ebay) but in general…
  • jw0752
    jw0752 over 8 years ago +5 suggested
    I agree with shabaz . This board is very difficult to do a nice clean job on. I believe that an improvement would have been to use a small gauge solid wire for the traces on the back side of the board…
Parents
  • DAB
    0 DAB over 8 years ago

    Hi Loic,

     

    In general, I think you are using too much solder.

     

    Remember, the goal is to bond the wire or lead to the pad.

     

    You first want to make sure you have a good physical connection by crimping the wire or lead around the pad.

     

    After that, you only need enough solder to show a good bond between the wire or lead to the pad.

     

    As you have observed, the big blobs of solder make the board look ugly and they can lead to possible shorts.

     

    So use only enough solder to gently coat the connection and you will have a better looking board.

     

    DAB

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • neliger
    0 neliger over 8 years ago in reply to DAB

    Thank you vary munch for the advise image

     

    I've some trouble to use less solder with the hot end of my soldering tool (looks like a 4mm screwdriver). I'll try to find thiner one, but it's hard to find compatible ones. Maybe I just need some practice.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • neliger
    0 neliger over 8 years ago in reply to DAB

    Thank you vary munch for the advise image

     

    I've some trouble to use less solder with the hot end of my soldering tool (looks like a 4mm screwdriver). I'll try to find thiner one, but it's hard to find compatible ones. Maybe I just need some practice.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • DAB
    0 DAB over 8 years ago in reply to neliger

    Yes, practice makes perfect.

     

    In tech school they had us solder for hours.

     

    My first big project after school required that I build cables for about 1000 wires.

     

    I soon developed a very good technic and there were no shorts in any of my cables and the cables survived a lot of yanking around when I installed them at the final site.

     

     

    So take your time, if you have a big soldering tip, then you can use a dry tip to wick the solder away by holding the tip under the solder joint and the excess solder will flow onto the tip and leave you with a nice clean joint.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer