Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Is this crap or acceptable work ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 9 answers
  • Subscribers 417 subscribers
  • Views 1594 views
  • Users 0 members are here
  • solder
  • diy
  • arduino
Related

Is this crap or acceptable work ?

e14 Contributor
e14 Contributor over 9 years ago

Hi to the community image

 

There is a long time since my last solder work. I've made a little thing today that looks like a wanted on the front, but (I think) looks like crap on the back lol

 

I would love to hear from all DIY lovers about this work : does it looks like I'll go to the electronic hell for having done this, or is this way to do it acceptable ?

 

For the record, this will be worn with a string around the neck, as it, just with some kapton on the back to protect cables.

 

Other question : is it insane to wear for a day an unprotected LiPo like this ?

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 9 years ago +5 verified
    Hi Loic, In general, I think you are using too much solder. Remember, the goal is to bond the wire or lead to the pad. You first want to make sure you have a good physical connection by crimping the wire…
  • shabaz
    shabaz over 9 years ago +5 suggested
    I agree with all the comments so far. Some things could be tweaked (like amount of solder, amount of heat, maybe even the component leads could be heavily oxidised if they are from ebay) but in general…
  • jw0752
    jw0752 over 9 years ago +4 suggested
    I agree with shabaz . This board is very difficult to do a nice clean job on. I believe that an improvement would have been to use a small gauge solid wire for the traces on the back side of the board…
Parents
  • ninjatrent
    0 ninjatrent over 9 years ago

    A solder wick can be used to remove excess solder. A small amount of solder rosin flux applied to both surfaces to be soldered will help the solder bond better. The rosin flux will free the surfaces of any oxidation and corrosion when heat is applied. For best results, use a small amount of solder to " tin " the solder tip, and tin each surface to be joined. So if you were to solder two wires together for instance, first dip each wire tip in rosin flux, then apply a small amount of solder to both points to be soldered. Same would apply to soldering on a PCB. Tinning the points to be soldered will make it easier. Especially if you are soldering different metal types together. Also, Lead-Free Solder requires a much higher heat than lead based solder.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to ninjatrent

    A solder wick can be used to remove excess solder

    I tend to show the pupils how gravity works, just as DAB talked about.

     

    During the teaching we discuss what a good solder joint should look like, and check their work. Any joints that are suspect we get them to straighten the lead (normally about 45deg) and then show that you can heat it up and drag the excess solder down the lead using gravity to help.

     

    Adafruit have a good soldering series.

    https://learn.adafruit.com/adafruit-guide-excellent-soldering/making-a-good-solder-joint

     

    Cheers

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to mcb1

    I'll look at that, thanks !

     

    I see some photos, this would be simpler for me to understand, as I don't get some words.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to mcb1

    I'll look at that, thanks !

     

    I see some photos, this would be simpler for me to understand, as I don't get some words.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 9 years ago in reply to e14 Contributor

    I see some photos

    Yes images are always better.

     

    We also teach pupils that not enough solder is as bad as too much, and to look for where it doesn't smoothly flow onto the wire or the board.

     

    The picture below shows the solder hasn't flowed onto the board and usually indicates not enough heat on the board, or solder running down the iron.

    The same can happen on the component end. It can be technique, but is often because of oxidation due to old components ..... as the others were suggesting.

     

    tools_Pad_Wetting.jpg

     

    Cheers

    mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer