Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Getting rid of batteries... simple question but what is the best way ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 6 answers
  • Subscribers 416 subscribers
  • Views 1590 views
  • Users 0 members are here
Related

Getting rid of batteries... simple question but what is the best way ?

redgreenblue
redgreenblue over 9 years ago

Hi Guys !

 

I have 4 door sensors with an arduino to have a simple sound trigger but also calculated how much peoples are getting by (helping a small museum in town).  I'll skip the details but the thing is I need to make theses connected to DC to avoid batteries changes (staff too busy). I figure the simple way to do it is using the arduino voltage out to the sensors.

 

I find this simple question complicated becuz I wonder if the current drain from the arduino will be enough for 4 sensors, so does capacitor might do the trick or if this is not the way to do it, I wonder if the AMP from the power supply should be higher ?

 

My calculation are that each sensor need 2x 1.5 volt batteries so it's approx. 3 volt @ 500mA

But I've tried the arduino output and 3.3volt does the trick, very good with one device.

 

Here a quick diagram of the setup.

If there is an expert in the room, stand up !

 

thank for your support

Element 14 is GREAT !!

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +2 suggested
    Hi, Can you give us a little more information on your sensors? The 500 mA seems awful high for a simple sensor. Do these devices light, ring or buzz? Are they being used as inputs to the Arduino. The 3…
  • jw0752
    jw0752 over 9 years ago in reply to redgreenblue +1 suggested
    Hi redgreenblue, Without knowing more details I would bring power from a separate 3 volt power supply and not try to use the 3.3 volts available on the Arduino. You could do this by having a separate wall…
  • jw0752
    jw0752 over 9 years ago in reply to redgreenblue +1 suggested
    Hi, Units that have 2 AA batteries for a power source will likely be designed to operate on much lower current draw than 500 mA. If not you would be replacing the batteries daily. AA batteries can deliver…
Parents
  • redgreenblue
    0 redgreenblue over 9 years ago

    Hi John,

     

    let's says the sensor are stand alone. They got sound, IR sensor and a reed switch (not 100% sure) what I do is simply catch the signal when someone is breaking the circuit by opening the door, the arduino is a 'calculator' in this setup. Since I already got wire going to them and becuz the museum has no wall plate anywhere to add a 'powersupply' we are back to the same setup, using wire to feed the 4 sensor to remplace the 8x AAA batteries.

     

    What do you think can be done ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • redgreenblue
    0 redgreenblue over 9 years ago

    Hi John,

     

    let's says the sensor are stand alone. They got sound, IR sensor and a reed switch (not 100% sure) what I do is simply catch the signal when someone is breaking the circuit by opening the door, the arduino is a 'calculator' in this setup. Since I already got wire going to them and becuz the museum has no wall plate anywhere to add a 'powersupply' we are back to the same setup, using wire to feed the 4 sensor to remplace the 8x AAA batteries.

     

    What do you think can be done ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 9 years ago in reply to redgreenblue

    Hi redgreenblue,

     

    Without knowing more details I would bring power from a separate 3 volt power supply and not try to use the 3.3 volts available on the Arduino. You could do this by having a separate wall wart and then using the wires you already have run or if the power supply for the Arduino is powerful enough you could use a regulator to bring its voltage to 3.3 volts and use that. If you are going to use a regulator I would recommend one of the Recon R78C3.3-1 which can efficiently convert the 9-12 volt power to the Arduino to 3.3 volts and can provide up to 1 amp of current. I am still assuming that the door sensors do not in fact draw a full 500 mA.

     

    http://www.newark.com/recom-power/r-78c3-3-1-0/dc-dc-converter-3-3w-3-3v-1a-sip/dp/62X9495?ost=R-78C3.3-1.0&scope=partnumberlookahead&exaMfpn=true&searchref=searchlookahead&searchView=table&iscrfnonsku=false&ddkey=http%3Aen-US%2FElement14_US%2Fw%2Fsearch

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer