Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino project housing help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 417 subscribers
  • Views 1152 views
  • Users 0 members are here
Related

Arduino project housing help

zewail97
zewail97 over 9 years ago

Hello everyone.

 

I'm new to the Arduino world and I need some help.

I've created my very first simple Arduino project [have a look]

image

It's really simple

 

It's using three sensors

1- MQ-5 for humidity sensing

2- LM35 for temperature sensing

3- BMP180 for pressure sensing

 

Let me explain the basic idea behind this project, every sensor has 2 leds, a green one and a red one, the greed led will be always on whenever the values of the sensors are in the right range

and the red led turns on when it over this range.

 

Now I want to cover this device to put it in the factory considering the following

1- It will be put in 100 degrees C

2- There will be dust

 

So here is what I need

 

1- A box to put the device in with lots of fans to keep the device cool in 100 degrees.

2- A cover for the wires to protect it from melting in 100 degrees.

3- A kind of texture to cover the LM35 and BMP180 sensors to prevent dust from going through them.

4- A kind of texture to cover the MQ-5 sensor to prevent dust but allow air to pass through.

 

Can you please suggest the best materials to get the job done perfectly?

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • gecoz
    gecoz over 9 years ago +2 suggested
    I'm not sure the sensors you are planning to use are suitable for your application. The LM35 will withstand 100C temperature, but definitely the BMP180 will not, as it is rated for the max temperature…
  • the-dubster
    the-dubster over 9 years ago in reply to gecoz +2 suggested
    Good point, I hadn't even considered questioning the sensor selection. I was thinking about the Temperature Sensor - I thought about how easy would it be to encapsulate it within a metal sleeve for protection…
  • the-dubster
    the-dubster over 9 years ago +1 suggested
    One tiny question about thermal management, is there going to be cool air fed to the unit? If not then fans will merely circulate 100 deg C air through the unit as it will take external (hot) air to replace…
Parents
  • the-dubster
    0 the-dubster over 9 years ago

    One tiny question about thermal management, is there going to be cool air fed to the unit? If not then fans will merely circulate 100 deg C air through the unit as it will take external (hot) air to replace exhausted (hot)air, little or no cooling will take place (there needs to be a temperature difference for cooling to occur).

     

    It is possible to find connecting cable that has a specification exceeding the maximum temperature you will face.

     

    Could the box be located remotely and the sensors (wire length permitting) be placed in the environment you wish to monitor?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • the-dubster
    0 the-dubster over 9 years ago

    One tiny question about thermal management, is there going to be cool air fed to the unit? If not then fans will merely circulate 100 deg C air through the unit as it will take external (hot) air to replace exhausted (hot)air, little or no cooling will take place (there needs to be a temperature difference for cooling to occur).

     

    It is possible to find connecting cable that has a specification exceeding the maximum temperature you will face.

     

    Could the box be located remotely and the sensors (wire length permitting) be placed in the environment you wish to monitor?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • zewail97
    0 zewail97 over 9 years ago in reply to the-dubster

    first, thanks for your answer.

     

    I hope this sketch answers your questions

    image

     

    Yes, there is going to be cool air fed to the unit as shown in the image.

     

    Yes, the box will be located remotely above the pipe and the sensors will be placed in the environment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • the-dubster
    0 the-dubster over 9 years ago in reply to zewail97

    Re: Enclosure.

     

    There are a quite a few options available, two common types are:

    PC (Polycarbonate) temperature range around -20°C to 140°C - it also has excellent insulating properties.

    ABS (Acrylonitrile Butadiene Styrene) again goes down to -20°C but not as hight as PC - also is not as tough or UV stable.

    You could always use an Aluminium (Aluminum) case - something to be aware of, it would need physical thermal insulation from the Pipe to prevent heat conduction, also, even if not physically attached, heat would be transferred by convection. A plastic enclosure would insulate from this effect better than a metal one.

    Re: Sensor mounting.

    I suppose you could just hang the sensors into the airflow with suitably heat rated cable, alternatively you could mount the sensors at the end of PC tubes, this would insulate the cable and provide a secure mounting point for the 3 sensors in the tube.

     

    Filtration is another area - one that will need a little more investigation. You would need to know the diameter of dust particles to best optimise the filtration material, you need to strike a fine line between blocking contaminants, maintaining uninterrupted airflow across the sensor, time between filter changes (it will clog) and thermal rating of the filtration material.

     

    Hopefully this will give you something to work with, and, as it's taken me so long to draft ALL my reply, I'll find out if anyone else has provided a solution for you when I 'Add Reply'.

     

    Regards

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • zewail97
    0 zewail97 over 9 years ago in reply to the-dubster

    That was very helpful, Thanks so much