Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Arduino Motor Driver vs Relay shield
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 414 subscribers
  • Views 2607 views
  • Users 0 members are here
  • relay controllers
  • motor contoller
  • arduino
Related

Arduino Motor Driver vs Relay shield

pjacobsen
pjacobsen over 8 years ago

Hey guys i'm new to this community! Was wondering if you had some insight for me.

I have (2) 12V 1A water pumps that I am trying to control via Arduino.

They only need to function in one state. (forward or reverse)

Are there benefits to using a motor driver for this application in terms of safety/efficiency?

Thanks in advanced,
Parker







  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +5 suggested
    Parker, Given a choice between a motor driver and a relay board for even simple (forward/reverse) driving of a motor, I would most likely chose the motor driver. In general, relays are mechanical devices…
  • genebren
    0 genebren over 8 years ago

    Parker,

     

    Given a choice between a motor driver and a relay board for even simple (forward/reverse) driving of a motor, I would most likely chose the motor driver.  In general, relays are mechanical devices that a subject to failure over time.  The contacts can get burned/tarnished, due to arching if precautions are not taken.  The added benefit of a full functional motor driver is that if your design changes, and you need something more than on/off control, you could add ramping controls to speed up and slow down the motor during starts and stops. If the cost between the two boards is not too much, I would likely choose the motor driver.

     

    Good luck with your project!

    Gene

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer