Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Detecting OFF state of an AC Load
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 36 replies
  • Answers 19 answers
  • Subscribers 418 subscribers
  • Views 6193 views
  • Users 0 members are here
Related

Detecting OFF state of an AC Load

anishkgt
anishkgt over 8 years ago

Hi All,

 

I am trying to switch on a LOAD from its OFF state by detecting a change in the voltage. Here the load is a MOT, the voltage at the primary is 1VAC when OFF.

 

My idea is to switch ON the MOT by detecting the voltage change at the primary when the Secondary are shorted. I can see a voltage drop of .5VAC when shorted. How can i monitor this voltage change with an Arduino.

 

My solution to the problem is shown below.

image

The Live of mains is connected to the MOT through the LIVE_LOAD in the schematic. During the OFF state the Optocoupler is triggered so that the 1VAC is seen by the Precision rectifier LT1078 and is rectified and send to the Analog pin A0 on the Arduino. With a code i could detect the voltage change and use it trigger the MOT again and at the same disable the optocoupler to break the circuit to the LT1078. Basically eliminating the need to press a switch two switch ON the MOT.

 

is there a better way to get this done. I was thinking of using the basic 1N4007 to convert the 1VAC to dc but that would be a problem when the MOT is switched ON allowing the mains 240VAC to flow through the DIODE.

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 8 years ago in reply to anishkgt +4 suggested
    1.3 V rms rectified is 1.8 Vdc minus the drop in a lightly loaded Schottky diode of 0.3 V is 1.5 V dc peak. The zener on the Schottky diode output is just to clamp the signal so it doesn't exceed your…
  • shabaz
    shabaz over 8 years ago in reply to anishkgt +4
    Electrodes? Important information like this is kind of missing in your question.. If you provide half the information, it's not a surprise that it wasn't understandable.
  • shabaz
    shabaz over 8 years ago +3 suggested
    The question (and the circuit) is not understandable I think : ( Could you rephrase the question, or draw a block diagram? The circuit doesn't make sense.
Parents
  • shabaz
    0 shabaz over 8 years ago

    The question (and the circuit) is not understandable I think : (

    Could you rephrase the question, or draw a block diagram? The circuit doesn't make sense.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago

    The question (and the circuit) is not understandable I think : (

    Could you rephrase the question, or draw a block diagram? The circuit doesn't make sense.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • anishkgt
    0 anishkgt over 8 years ago in reply to shabaz

    The question is simply an auto-switch ON for a MOT that i had in mind and now as a schematic seeking second opinion from the pro's.

     

    The CS enable on the optocoupler is connected to an Arduino which is used to switch on and off the circuit that senses the state of the LOAD. The other side is the part is a precision rectifier that rectifies the 1VAC to DC so that the Arduino can work with it.

     

     

    Hope this adds more clarity.