Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum ESP8266 connection to Uno R3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 6 answers
  • Subscribers 415 subscribers
  • Views 2252 views
  • Users 0 members are here
Related

ESP8266 connection to Uno R3

gam3t3ch
gam3t3ch over 8 years ago

Will a Esp8266 work on a uno r3 without resistors?

This is the one I am using the ESP-01  I don't really want to buy the board to go with it if I don't need it.

Thanks in advance.  similar to the below is what I have.

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • gam3t3ch
    gam3t3ch over 8 years ago in reply to genebren +3 suggested
    Just found a I2C Logic Level Converter Bi-Directional Module 5V to 3.3V in my bin whats the odds. Should do the trick.
  • ntewinkel
    ntewinkel over 8 years ago +2 suggested
    The ESP-01 is officially a 3.3v device, but I've heard of people just hooking them up straight to the 5v pins (maybe powered by the 3.3v Uno pin, not sure). To be safe you'll probably need a level-shifter…
  • genebren
    genebren over 8 years ago +2 suggested
    Note: The ESP8266 Module is not capable of 5-3V logic shifting and will require an external Logic Level Converter . Please do not power it directly from your 5V dev board. Note: The ESP8266 Module is not…
Parents
  • chris_b
    0 chris_b over 8 years ago

    Arduino TX -> ESP RX and Arduino -> ESP RESET through the level shifter

     

    ESP TX -> Arduino RX is fine, 3.3v is good enough for a 'high' signal

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to chris_b

    oh right, I keep forgetting about the reset!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to chris_b

    oh right, I keep forgetting about the reset!