Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum ESP8266 connection to Uno R3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 6 answers
  • Subscribers 415 subscribers
  • Views 2244 views
  • Users 0 members are here
Related

ESP8266 connection to Uno R3

gam3t3ch
gam3t3ch over 8 years ago

Will a Esp8266 work on a uno r3 without resistors?

This is the one I am using the ESP-01  I don't really want to buy the board to go with it if I don't need it.

Thanks in advance.  similar to the below is what I have.

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • gam3t3ch
    gam3t3ch over 8 years ago in reply to genebren +3 suggested
    Just found a I2C Logic Level Converter Bi-Directional Module 5V to 3.3V in my bin whats the odds. Should do the trick.
  • ntewinkel
    ntewinkel over 8 years ago +2 suggested
    The ESP-01 is officially a 3.3v device, but I've heard of people just hooking them up straight to the 5v pins (maybe powered by the 3.3v Uno pin, not sure). To be safe you'll probably need a level-shifter…
  • genebren
    genebren over 8 years ago +2 suggested
    Note: The ESP8266 Module is not capable of 5-3V logic shifting and will require an external Logic Level Converter . Please do not power it directly from your 5V dev board. Note: The ESP8266 Module is not…
Parents
  • genebren
    0 genebren over 8 years ago

    Note: The ESP8266 Module is not capable of 5-3V logic shifting and will require an external Logic Level Converter. Please do not power it directly from your 5V dev board.Note: The ESP8266 Module is not capable of 5-3V logic shifting and will require an Wesley,

     

    From the Sparkfun page for the ESP8266 module:

     

    Note: The ESP8266 Module is not capable of 5-3V logic shifting and will require an external Logic Level Converter. Please do not power it directly from your 5V dev board.

     

    So be careful.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to genebren

    Wesley,

     

    Wow, that got a little messed up.

     

    Just another thought.  You could modify you Uno to operate at 3.3V by replacing the 5.0 regulator on the Uno board with a 3.3V one.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gam3t3ch
    0 gam3t3ch over 8 years ago in reply to genebren

    Just found a I2C Logic Level Converter Bi-Directional Module 5V to 3.3V in my bin whats the odds.  Should do the trick.

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • chris_b
    0 chris_b over 8 years ago in reply to gam3t3ch

    Take care of the 3.3 supply also, the ESP can draw up to 320mA at startup.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to genebren

    >You could modify you Uno to operate at 3.3V by replacing the 5.0 regulator on the Uno board with a 3.3V one.

     

    Could you supply regulated 3.3v to the 5v pin directly?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gam3t3ch
    0 gam3t3ch over 8 years ago in reply to ntewinkel

    So should I be running the rx and tx through the board or just the 5v - 3.3v?  or am I way off on that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to gam3t3ch

    I would power the ESP board from the 3.3v pin of the Uno (to ESP vcc), and run rx/tx through that little level shifter board. If I recall correctly, the level shifter board will have 5v power input on the Uno side, and a 3.3v power input on the ESP side. So I'd connect those up to the Uno 5v and 3.3v pins respectively.

     

    Looks like this project on Hackster shows all the details: https://www.hackster.io/circuito-io-team/simple-arduino-uno-esp-8266-integration-dba10b

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to gam3t3ch

    I would power the ESP board from the 3.3v pin of the Uno (to ESP vcc), and run rx/tx through that little level shifter board. If I recall correctly, the level shifter board will have 5v power input on the Uno side, and a 3.3v power input on the ESP side. So I'd connect those up to the Uno 5v and 3.3v pins respectively.

     

    Looks like this project on Hackster shows all the details: https://www.hackster.io/circuito-io-team/simple-arduino-uno-esp-8266-integration-dba10b

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer