Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Laser tripwire assistance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 415 subscribers
  • Views 473 views
  • Users 0 members are here
Related

Laser tripwire assistance

otanoob
otanoob over 8 years ago

I've been trying to setup a laser tripwire as a fantasy project. The sketch I'm using looks like this

 

[code]

 

int ldrPin = A4; // the cell and 10K: pulldovn are connected to a0

int sirenPin = 11; //pin 3 selected!!

int ledPin = A0;

long ldrValue1, ldrValue2;

void setup(void) {

  pinMode (sirenPin, OUTPUT); // set the siren pin as output

  pinMode (ledPin, OUTPUT); // set the siren pin as output

  pinMode (ldrPin, INPUT); // set the siren pin as output

  //Serial.begin(9600);

}

void loop(void) {

  ldrValue1 = analogRead(ldrPin);

  delay(10);

  ldrValue2 = analogRead(ldrPin);

  if (ldrValue1 - ldrValue2 > 20) {

    digitalWrite(sirenPin, HIGH);

    digitalWrite(ledPin, HIGH);

    delay(1000);

  }

  else {

    digitalWrite(sirenPin, LOW);

    digitalWrite(ledPin, LOW);

  }

  //Serial.print("Analog reading = ");

  //Serial.println(ldrValue1); // the raw analog reading

}

[/code]

 

My issue seems to be with the hardware. I was told a 1k resistor would suffice for the ldr I'm using .It all worked for an hour, then I attempted to extend the ldr with jumper wires and it stopped functioning. Any ideas?

 

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +3 suggested
    You may wish to revise where things are actually connected. int ldrPin = A4; // the cell and 10K: pulldovn are connected to a0 int sirenPin = 11; //pin 3 selected!! int ledPin = A0; long ldrValue1, ldrValue2;…
  • fmilburn
    fmilburn over 8 years ago +1 suggested
    Hi Joseph, If you are using a breadboard, check all connections to make sure they are good. If you have a digital multimeter you can check for continuity. Turn on the serial print and see if there is a…
Parents
  • mcb1
    0 mcb1 over 8 years ago

    You may wish to revise where things are actually connected.

     

    int ldrPin = A4; // the cell and 10K: pulldovn are connected to a0
    int sirenPin = 11; //pin 3 selected!!
    int ledPin = A0;
    long ldrValue1, ldrValue2;
    void setup(void) {
      pinMode (sirenPin, OUTPUT); // set the siren pin as output
      pinMode (ledPin, OUTPUT); // set the siren pin as output
      pinMode (ldrPin, INPUT); // set the siren pin as output
      //Serial.begin(9600);
    }
    void loop(void) {
      ldrValue1 = analogRead(ldrPin);
      delay(10);
      ldrValue2 = analogRead(ldrPin);
      if (ldrValue1 - ldrValue2 > 20) {
        digitalWrite(sirenPin, HIGH);
        digitalWrite(ledPin, HIGH);
        delay(1000);
      }
      else {
        digitalWrite(sirenPin, LOW);
        digitalWrite(ledPin, LOW);
      }
      //Serial.print("Analog reading = ");
      //Serial.println(ldrValue1); // the raw analog reading
    }

     

    Line 01 says that the LDR will connect to A0, yet the declaration is A4

    Line 02 says it will be D3 yet the declaration is D11

    Line 03 has the Led on A0.

     

    Not sure where you got the code from but reading the LDR 10mS apart is probably going to give the same value.

    So I suspect it will never meet the true condition in Line 14.

     

     

    Not that it will matter but the analogue vaue reading is a number between 0 and 1023, so it doen't need to be decalred as a long, and int will handle it just as well.

     

     

    Can you confirm the connections .... maybe a good well focused picture or two.

    Otherwise it looks like it should work.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago

    You may wish to revise where things are actually connected.

     

    int ldrPin = A4; // the cell and 10K: pulldovn are connected to a0
    int sirenPin = 11; //pin 3 selected!!
    int ledPin = A0;
    long ldrValue1, ldrValue2;
    void setup(void) {
      pinMode (sirenPin, OUTPUT); // set the siren pin as output
      pinMode (ledPin, OUTPUT); // set the siren pin as output
      pinMode (ldrPin, INPUT); // set the siren pin as output
      //Serial.begin(9600);
    }
    void loop(void) {
      ldrValue1 = analogRead(ldrPin);
      delay(10);
      ldrValue2 = analogRead(ldrPin);
      if (ldrValue1 - ldrValue2 > 20) {
        digitalWrite(sirenPin, HIGH);
        digitalWrite(ledPin, HIGH);
        delay(1000);
      }
      else {
        digitalWrite(sirenPin, LOW);
        digitalWrite(ledPin, LOW);
      }
      //Serial.print("Analog reading = ");
      //Serial.println(ldrValue1); // the raw analog reading
    }

     

    Line 01 says that the LDR will connect to A0, yet the declaration is A4

    Line 02 says it will be D3 yet the declaration is D11

    Line 03 has the Led on A0.

     

    Not sure where you got the code from but reading the LDR 10mS apart is probably going to give the same value.

    So I suspect it will never meet the true condition in Line 14.

     

     

    Not that it will matter but the analogue vaue reading is a number between 0 and 1023, so it doen't need to be decalred as a long, and int will handle it just as well.

     

     

    Can you confirm the connections .... maybe a good well focused picture or two.

    Otherwise it looks like it should work.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer