Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Laser tripwire assistance
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 415 subscribers
  • Views 472 views
  • Users 0 members are here
Related

Laser tripwire assistance

otanoob
otanoob over 8 years ago

I've been trying to setup a laser tripwire as a fantasy project. The sketch I'm using looks like this

 

[code]

 

int ldrPin = A4; // the cell and 10K: pulldovn are connected to a0

int sirenPin = 11; //pin 3 selected!!

int ledPin = A0;

long ldrValue1, ldrValue2;

void setup(void) {

  pinMode (sirenPin, OUTPUT); // set the siren pin as output

  pinMode (ledPin, OUTPUT); // set the siren pin as output

  pinMode (ldrPin, INPUT); // set the siren pin as output

  //Serial.begin(9600);

}

void loop(void) {

  ldrValue1 = analogRead(ldrPin);

  delay(10);

  ldrValue2 = analogRead(ldrPin);

  if (ldrValue1 - ldrValue2 > 20) {

    digitalWrite(sirenPin, HIGH);

    digitalWrite(ledPin, HIGH);

    delay(1000);

  }

  else {

    digitalWrite(sirenPin, LOW);

    digitalWrite(ledPin, LOW);

  }

  //Serial.print("Analog reading = ");

  //Serial.println(ldrValue1); // the raw analog reading

}

[/code]

 

My issue seems to be with the hardware. I was told a 1k resistor would suffice for the ldr I'm using .It all worked for an hour, then I attempted to extend the ldr with jumper wires and it stopped functioning. Any ideas?

 

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +3 suggested
    You may wish to revise where things are actually connected. int ldrPin = A4; // the cell and 10K: pulldovn are connected to a0 int sirenPin = 11; //pin 3 selected!! int ledPin = A0; long ldrValue1, ldrValue2;…
  • fmilburn
    fmilburn over 8 years ago +1 suggested
    Hi Joseph, If you are using a breadboard, check all connections to make sure they are good. If you have a digital multimeter you can check for continuity. Turn on the serial print and see if there is a…
Parents
  • fmilburn
    0 fmilburn over 8 years ago

    Hi Joseph,

     

    If you are using a breadboard, check all connections to make sure they are good.  If you have a digital multimeter you can check for continuity.  Turn on the serial print and see if there is a reading on the analog pin.  Did you change the resistor from when it was working?  I would not expect a jumper to make a difference if there is a good connection.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 8 years ago

    Hi Joseph,

     

    If you are using a breadboard, check all connections to make sure they are good.  If you have a digital multimeter you can check for continuity.  Turn on the serial print and see if there is a reading on the analog pin.  Did you change the resistor from when it was working?  I would not expect a jumper to make a difference if there is a good connection.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer