Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Help. I need the reverse of zero crossing
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 4 answers
  • Subscribers 415 subscribers
  • Views 1865 views
  • Users 0 members are here
  • inrush
  • programing
  • arduino
Related

Help. I need the reverse of zero crossing

phoenixcomm
phoenixcomm over 8 years ago

Ok, I need some hunk of code to detect the peek not the zero crossing. ( this is the solution).

Problem: Toroid based power supply have inrush current problems. As when you turn on the power switch,

it is a random chance where on the sine wave it will be.

You can not start this a zero crossing as that is the Imax and will blow your fuse. image

This solution must be only a primary side problem. I was thinking of a relay but a small triac is much faster.

Thanks

Cris

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 8 years ago +3 suggested
    Why do you need code - the simplest trick is to use an NTC current limiter. These people have a lovely web site: https://www.ametherm.com/ If you have to do it in code it might be easier to detect zero…
  • abrain
    abrain over 7 years ago in reply to phoenixcomm +3 verified
    Yes, sorry Cris, I don’t think I explained it very well. If you’re measuring the voltage (which I think you must be to find the zero crossing) then work out how much that voltage changed from the last…
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to michaelkellett +1 suggested
    I have seen current limiters like Ametherms before. But the problem is that I have three toroidal power transformers, and for the first 20ms or so they draw I max so the idea is to turn them on one at…
Parents
  • michaelkellett
    0 michaelkellett over 8 years ago

    Why do you need code - the simplest trick is to use an NTC current limiter. These people have a lovely web site:

     

    https://www.ametherm.com/

     

    If you have to do it in code it might be easier to detect zero crossings and then add a suitable time (phase) delay to locate the next peak.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 8 years ago

    Why do you need code - the simplest trick is to use an NTC current limiter. These people have a lovely web site:

     

    https://www.ametherm.com/

     

    If you have to do it in code it might be easier to detect zero crossings and then add a suitable time (phase) delay to locate the next peak.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • phoenixcomm
    0 phoenixcomm over 8 years ago in reply to michaelkellett

    I have seen current limiters like Ametherms before. But the problem is that I have three toroidal power transformers, and for the first 20ms or so they draw Imax so the idea is to turn them on one at a time about one second apart. I like your idea about using a delay from zero crossing.

    Since we know that (T=1/60) 1/60Hz = 0.0166666667 then by using T/2 = 0.00833333335 now I will have to check this on my scope and most likely fudge the result as I really want this to fire just at the start of the bottom of the peak curve ie just before the top. and on the way down.

     

    thanks for the help

    Great answer!

    Cris H.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer