Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Pin-throughs with TFT on Uno?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 414 subscribers
  • Views 1296 views
  • Users 0 members are here
  • tft
  • touchscreen
  • arduino
Related

Pin-throughs with TFT on Uno?

Andrew J
Andrew J over 7 years ago

I'm getting a little confused on how some of the shields work with an Arduino Uno.  I want to be able to connect a touchscreen and, at the same time, drive some ADCs and DACs.  Take as an example this screen from Adafruit (but the question isn't really specific to these, the Newhaven ones look good too):

 

https://www.adafruit.com/product/1651

 

It says it leaves digital pins 2,3,5,6,7 and analog pins 0-5 for use and yet all the pictures show that the shield completely covers the UNO with no passthroughs.  I can't even see how I can attach to the 5v and GND pins to power the thing (I don't want to use the USB or DC adapter once it's in an enclosure!  I've done very little with an Arduino to date and never used a shield so I'm unsure how these things work - could someone advise please?

 

Something like a Nextion screen looks very useful but I only have a Mac so can't use the required editor program.  If there's something similar available that I haven't been able to find I'd be interested in knowing.

 

Thanks,

 

Andrew

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 7 years ago +3 verified
    Hi Andrew, Shields are for solving various problems, but as you've observed, can cause problems when you want to use multiple shields simultaneously. There are some shields that allow stacking, so that…
  • beacon_dave
    beacon_dave over 7 years ago +2 suggested
    You could use a Proto Shield between the UNO and the TFT shield for your additional connectivity. https://www.adafruit.com/product/2077
  • shabaz
    shabaz over 7 years ago in reply to Andrew J +2 suggested
    Hi Andrew, If you've got ready-made dupont wires, that would work. Optionally, if you wanted to, you could buy the type of plastic shells linked earlier, and they have a tab, so you can remove the single…
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Andrew,

     

    Shields are for solving various problems, but as you've observed, can cause problems when you want to use multiple shields simultaneously. There are some shields that allow stacking, so that may be an option (not always possible).

    Another way to solve the physical issue of attaching more than two connections together, is to assemble some cables to attach to the shields (i.e. do not plug them on the Arduino directly).

    Here's one example in the photo below (this is not using an Arduino, but it's the same principle). The photo below shows an Arduino-like board (black, bottom-left) but other boards are not plugged on top. Instead, cables are used to connect to the green boards in the photo.

    image

    To make the cables, you need thin wire (e.g. 10/0.1 wire), 0.1" header pin crimp sockets0.1" header pin crimp sockets, and a crimping toolcrimping tool. Plastic shellsPlastic shells are also available.

    You'll still need to make sure there are no clashes. If you run out of useful Arduino Uno pins then you may need a different Arduino, or consider different ways (e.g. using a port expander chip (google will provide more information on this, and your code will need to change if you use it).

    Here is a closeup of what the tool does (this is not the same crimp socket as the one linked above, but similar). The photo shows two wires into the same crimp socket (stripped cat-5 cable!).

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago

    Hi Andrew,

     

    Shields are for solving various problems, but as you've observed, can cause problems when you want to use multiple shields simultaneously. There are some shields that allow stacking, so that may be an option (not always possible).

    Another way to solve the physical issue of attaching more than two connections together, is to assemble some cables to attach to the shields (i.e. do not plug them on the Arduino directly).

    Here's one example in the photo below (this is not using an Arduino, but it's the same principle). The photo below shows an Arduino-like board (black, bottom-left) but other boards are not plugged on top. Instead, cables are used to connect to the green boards in the photo.

    image

    To make the cables, you need thin wire (e.g. 10/0.1 wire), 0.1" header pin crimp sockets0.1" header pin crimp sockets, and a crimping toolcrimping tool. Plastic shellsPlastic shells are also available.

    You'll still need to make sure there are no clashes. If you run out of useful Arduino Uno pins then you may need a different Arduino, or consider different ways (e.g. using a port expander chip (google will provide more information on this, and your code will need to change if you use it).

    Here is a closeup of what the tool does (this is not the same crimp socket as the one linked above, but similar). The photo shows two wires into the same crimp socket (stripped cat-5 cable!).

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Connecting via wires to the screen/shield instead of plugging in directly!?!  That is just way too obvious and simple, no wonder I didn't think of it image.  Would dupont-type wires work do you know - I have enough of those to hand already to save making more up.

     

    I actually don't have more than one shield: just the UNO to connect to a touchscreen TFT for UI/control and then analog and digital pins to ADC and DAC on a separate PCB. 

     

    Thanks for your help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 7 years ago in reply to Andrew J

    Hi Andrew,

     

    If you've got ready-made dupont wires, that would work. Optionally, if you wanted to, you could buy the type of plastic shells linked earlier, and they have a tab, so you can remove the single plastic shells on your dupont wires, and insert into (say) a 8-way or 10-way shell. It's not essential, but handy sometimes. The crimp tool is cheap ($36USD/£20GBP+VAT), so longer term you might want to buy that anyway, to roll your own custom-length cables.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J over 7 years ago in reply to shabaz

    Agreed - and I probably want to keep those wires as short as possible.