Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum The Arduino Vidor4000: is there a new IDE?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 1767 views
  • Users 0 members are here
  • arduino_mkr
  • vidor 4000
Related

The Arduino Vidor4000: is there a new IDE?

14rhb
14rhb over 7 years ago

It was just over a year ago now that I spotted the new Arduino Vidor4000 FPGA board and decided to get one E14blog https://www.element14.com/community/message/244346/l/re-arduino-the-mkr-contest-series-show-us-how-you-would-use-the-arduino-mkr-line#244346

 

I ran through the limited demonstrations but found it was far from hands on FPGA and almost impossible to understand how to create anything else. The Webinars from Massimo seemed promising as he talked about the software team creating a new GUI that would allow the Vidor4000 to be graphically programmed - that sounded idea and just the sort of thing I was after...a simple drag and drop experience.

 

Element14 held a competition where members also used this board but I didn't see much apart from the pre-built libraries being used - please correct me if I'm wrong there.

 

My Vidor4000 sat on the shelf image watching the sun rise and set, the trees budding, setting seed and the leaves falling again.

 

Last night I logged into the Arduino website assuming by now there would be some new IDE specifically for the Vidor4000 and the FPGA aspects but couldn't find anything. And the documentation for the board also seemed to be stagnant with the HDMI display example and little else.

 

I'd be grateful if someone can point me to any useful articles on making my own blocks in HDL or some new graphical IDE that I've completely missed being launched over the last year.

  • Sign in to reply
  • Cancel

Top Replies

  • 14rhb
    14rhb over 7 years ago in reply to jomoenginer +3
    Thanks jomoenginer . I'll check those links out. I'm doing some work at one end of the FPGA scale using a Xilinx ZC702 and that is really hard work, although rewarding. I had hoped to do some fun stuff…
  • tariq.ahmad
    tariq.ahmad over 7 years ago +2 suggested
    Hi 14rhb , I posted some reference links that I found in the following doc: Arduino MKR VIDOR 4000 Pinout, SAMD21 Pin Mapping, Tech Specs, EAGLE Files, Github, Schematics, Reference Links, FAQ, and More…
  • 14rhb
    14rhb over 7 years ago in reply to tariq.ahmad +2
    Jackpot . Thank you tariq.ahmad . Those links to systemes-embarques.fr detail using Verilog code in Quartus II to program the FPGA (an Intel Cyclone 10 10CL016) and the examples are just the sort of simple…
Parents
  • jomoenginer
    0 jomoenginer over 7 years ago

    Yeah, this is a common issue with the MKR Vidor 4000.  I think Arduino jumped too soon with the device and now are relying on the Arduino Community and beyond to fill in the gaps.

     

    I tried to work on some of the FPGA stuff with my Vidor Scout but ran into too many road blocks. I should get back to messing with it again though:

    https://www.element14.com/community/community/project14/programmable-logic/blog/2019/06/23/vidorscout-mkr-vidor-4000-mobile-robot-vidorbitstream-compile

     

    You might find some answers on the Arduino Forum, but it is very limiting though.

    https://forum.arduino.cc/index.php?board=125.0

     

    Your best bet would be to check out the GitHub repo and perhaps follow some of the folks that have forked the Arduino code since they seem to be ones moving ahead with some development with the board.

    https://github.com/vidor-libraries

     

    Good luck.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • 14rhb
    0 14rhb over 7 years ago in reply to jomoenginer

    jomoenginer Is the software you detail for your Vidor Scout also using Quartus 2, just from the command line rather than GUI? Looks very promising, thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 14rhb
    0 14rhb over 7 years ago in reply to jomoenginer

    jomoenginer Is the software you detail for your Vidor Scout also using Quartus 2, just from the command line rather than GUI? Looks very promising, thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jomoenginer
    0 jomoenginer over 7 years ago in reply to 14rhb

    Yes, it uses Quartus II Lite and NIOS II.

     

    This is a good reference for code that works:

    https://github.com/MinatsuT/VidorBitstream_GFX_HW

     

    The thing to keep in mind is that unless you are using USB Blaster via JTAG or software libraries, the FPGA code load is from the Arduino IDE.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer