Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum ESP32-CAM Help!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 416 subscribers
  • Views 4673 views
  • Users 0 members are here
Related

ESP32-CAM Help!

arduino420
arduino420 over 6 years ago

I ordered a 4 pack of ESP32-CAM (https://amzn.to/3355sWO) and I've been trying to load the CameraWebServer example file (only modified WIFI settings, and camera model definition) using the Arduino IDE and I keep getting the fatal error: "Failed to connect to ESP32: Timed out waiting for packet header".

 

 

I've connected my FTDI adapter (https://bit.ly/2qkebHA) using RandomNerd's wiring diagram (https://bit.ly/333Qtwu) and settings (board/partition scheme/port) and tried both 5v and 3.3v with no success - each time is a fatal error... I tried loading with *AND *without connecting IO0 to GND but no luck.

 

 

Is there anyone that can help provide some additional guidance? (I tried all 4 ESP32-CAM modules but received same fatal error for all). I should also mention that I'm able to load firmware into Arduino Pro Mini using the same FTDI adapter so I know that adapter works.image

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +2 suggested
    What is powering the ESP32 board? In your photo (you can insert them in-line like this, makes it much easier to follow): 5873.contentimage_205327.jpg The red wire looks as if it is connected to an pin…
  • ralphjy
    ralphjy over 6 years ago +2 suggested
    I agree with Shabaz that if you have it hooked up as in your picture - that is incorrect. It appears that you can select either 5V or 3.3V output from your FTDI adapter. Based on your selection you should…
  • mp2100
    mp2100 over 6 years ago in reply to arduino420 +2
    Hoo boy, 3 out of 4 bad. I guess that’s why they sell a 4-pack? So you get one that works. 2664.contentimage_402.png
Parents
  • shabaz
    0 shabaz over 6 years ago

    What is powering the ESP32 board? In your photo (you can insert them in-line like this, makes it much easier to follow):

    5873.contentimage_205327.jpg

    The red wire looks as if it is connected to an pin that is a voltage output on the ESP board, not a voltage input, and I couldn't see any other power wiring to the ESP board.

    There's not a lot of info on the Amazon page, but that pin with the red wire is indicated as P_OUT:

    1663.contentimage_205328.jpg

    Is the USB UART board supplying power on that pin? Or does it expect a voltage level on that pin so that it knows the logic level for the UART?

    I think these things need to be investigated, preferably with a multimeter, and checking whatever web page or documentation you have on the USB UART board too, because it's not possible to know from just the photo : (

    The USB UART page has no information, and a photo where the text is unreadable : (

    3730.contentimage_205329.jpg

    Amazon and Microcenter are maybe not the best places to buy this stuff, if this is the best they can do : (

    I think online stores like Seeed or Adafruit may be better for these types of products (I have not checked), if Farnell/Newark don't stock them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    What is powering the ESP32 board? In your photo (you can insert them in-line like this, makes it much easier to follow):

    5873.contentimage_205327.jpg

    The red wire looks as if it is connected to an pin that is a voltage output on the ESP board, not a voltage input, and I couldn't see any other power wiring to the ESP board.

    There's not a lot of info on the Amazon page, but that pin with the red wire is indicated as P_OUT:

    1663.contentimage_205328.jpg

    Is the USB UART board supplying power on that pin? Or does it expect a voltage level on that pin so that it knows the logic level for the UART?

    I think these things need to be investigated, preferably with a multimeter, and checking whatever web page or documentation you have on the USB UART board too, because it's not possible to know from just the photo : (

    The USB UART page has no information, and a photo where the text is unreadable : (

    3730.contentimage_205329.jpg

    Amazon and Microcenter are maybe not the best places to buy this stuff, if this is the best they can do : (

    I think online stores like Seeed or Adafruit may be better for these types of products (I have not checked), if Farnell/Newark don't stock them.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer