Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum ESP32-CAM Help!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 416 subscribers
  • Views 4673 views
  • Users 0 members are here
Related

ESP32-CAM Help!

arduino420
arduino420 over 6 years ago

I ordered a 4 pack of ESP32-CAM (https://amzn.to/3355sWO) and I've been trying to load the CameraWebServer example file (only modified WIFI settings, and camera model definition) using the Arduino IDE and I keep getting the fatal error: "Failed to connect to ESP32: Timed out waiting for packet header".

 

 

I've connected my FTDI adapter (https://bit.ly/2qkebHA) using RandomNerd's wiring diagram (https://bit.ly/333Qtwu) and settings (board/partition scheme/port) and tried both 5v and 3.3v with no success - each time is a fatal error... I tried loading with *AND *without connecting IO0 to GND but no luck.

 

 

Is there anyone that can help provide some additional guidance? (I tried all 4 ESP32-CAM modules but received same fatal error for all). I should also mention that I'm able to load firmware into Arduino Pro Mini using the same FTDI adapter so I know that adapter works.image

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +2 suggested
    What is powering the ESP32 board? In your photo (you can insert them in-line like this, makes it much easier to follow): 5873.contentimage_205327.jpg The red wire looks as if it is connected to an pin…
  • ralphjy
    ralphjy over 6 years ago +2 suggested
    I agree with Shabaz that if you have it hooked up as in your picture - that is incorrect. It appears that you can select either 5V or 3.3V output from your FTDI adapter. Based on your selection you should…
  • mp2100
    mp2100 over 6 years ago in reply to arduino420 +2
    Hoo boy, 3 out of 4 bad. I guess that’s why they sell a 4-pack? So you get one that works. 2664.contentimage_402.png
Parents
  • ralphjy
    0 ralphjy over 6 years ago

    I agree with Shabaz that if you have it hooked up as in your picture - that is incorrect.  It appears that you can select either 5V or 3.3V output from your FTDI adapter.  Based on your selection you should connect to either the 5V or 3.3V pin of the ESP32cam (the red POW pins at the bottom of the picture).  The RandomNerd tutorial shows a connection to the 3.3V.

     

    I should also mention that I’ve had brownout issues using the FTDI adapter to power the board via the computer USB port.  For development I use a separate 5V supply to power the ESP32cam.  If you do that just remember to connect GND in addition to the TX and RX pins when you connect the UART.  The brownouts only occur when using WiFi or Bluetooth (higher current) and will cause intermittent reboots.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ralphjy
    0 ralphjy over 6 years ago

    I agree with Shabaz that if you have it hooked up as in your picture - that is incorrect.  It appears that you can select either 5V or 3.3V output from your FTDI adapter.  Based on your selection you should connect to either the 5V or 3.3V pin of the ESP32cam (the red POW pins at the bottom of the picture).  The RandomNerd tutorial shows a connection to the 3.3V.

     

    I should also mention that I’ve had brownout issues using the FTDI adapter to power the board via the computer USB port.  For development I use a separate 5V supply to power the ESP32cam.  If you do that just remember to connect GND in addition to the TX and RX pins when you connect the UART.  The brownouts only occur when using WiFi or Bluetooth (higher current) and will cause intermittent reboots.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer