Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Port registers Nano Every (ATmega4809)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 413 subscribers
  • Views 6505 views
  • Users 0 members are here
  • atmega4809
  • nano every
  • registers
  • bitwise
Related

Port registers Nano Every (ATmega4809)

luislabmo
luislabmo over 6 years ago

Can someone illustrate -or- point me in the right direction on how to manipulate port registers in the Nano Every (ATmega4809)?. - I'm using the Arduino IDE

The port manipulation described here for the ATmega328p/ATmega168 works as follows and works well for me in the Arduino Pro Mini and ATmega48;

DDRD |= B11110000; // sets ATmega digital pins 7 to 4 as Outputs
PORTD = B10010000; // sets digital pins 7,4 HIGH

 

When I try the equivalent with the Nano Every (ATmega4809) it seems the pin mapping is completely different

VPORTD.DIR |= B11110000;
VPORTD.OUT = B11110000;

 

I'm using bit-wise operations as my plan is to replicate the same in the Nano Every without emulation -if possible- so I can manipulate many digital/analog pins at once with one instruction (avoiding having to do it for each GPIO at a time)

 

Thanks,

 

Luis

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +4 verified
    Hi Luis, It should be the same, however the pins would be the Port D pins for bits 4-7, which won't necessarily be labelled D4-7 on the Arduino. For example, the port D bit 4 is labelled D20 (see the red…
  • luislabmo
    luislabmo over 6 years ago in reply to shabaz +1
    Thank you Shabaz, it worked as you described!. It was a bummer for me that the pins are all spread and couldn't managed to find a quantity enough grouped under the same register for my intended use. Thanks…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Luis,

     

    It should be the same, however the pins would be the Port D pins for bits 4-7, which won't necessarily be labelled D4-7 on the Arduino. For example, the port D bit 4 is labelled D20 (see the red arrows in the diagram below). So setting Port D bits 4-7 would actually set D20, D21, AREF .

    I have not got an Arduino Every so this is just based on what I'd expect to occur though.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    Hi Luis,

     

    It should be the same, however the pins would be the Port D pins for bits 4-7, which won't necessarily be labelled D4-7 on the Arduino. For example, the port D bit 4 is labelled D20 (see the red arrows in the diagram below). So setting Port D bits 4-7 would actually set D20, D21, AREF .

    I have not got an Arduino Every so this is just based on what I'd expect to occur though.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • luislabmo
    0 luislabmo over 6 years ago in reply to shabaz

    Thank you Shabaz, it worked as you described!.

     

    It was a bummer for me that the pins are all spread and couldn't managed to find a quantity enough grouped under the same register for my intended use.

     

    Thanks a lot for your help.

     

    Luis

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Leopard347
    0 Leopard347 over 3 years ago in reply to shabaz

    But there is no PD6

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to Leopard347

    I'm not sure what the issue is, it's normal for boards and even microcontrollers to be missing certain GPIO pins: not all need make their way out to physical pins based on the type of package. The register addresses often still reference those absent pins, it is up to the user to ignore those bits in the registers.

    I've not used this microcontroller or board, and I'm mobile with no easy access to the datasheet, so I could be totally wrong.