Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Port registers Nano Every (ATmega4809)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 413 subscribers
  • Views 6505 views
  • Users 0 members are here
  • atmega4809
  • nano every
  • registers
  • bitwise
Related

Port registers Nano Every (ATmega4809)

luislabmo
luislabmo over 6 years ago

Can someone illustrate -or- point me in the right direction on how to manipulate port registers in the Nano Every (ATmega4809)?. - I'm using the Arduino IDE

The port manipulation described here for the ATmega328p/ATmega168 works as follows and works well for me in the Arduino Pro Mini and ATmega48;

DDRD |= B11110000; // sets ATmega digital pins 7 to 4 as Outputs
PORTD = B10010000; // sets digital pins 7,4 HIGH

 

When I try the equivalent with the Nano Every (ATmega4809) it seems the pin mapping is completely different

VPORTD.DIR |= B11110000;
VPORTD.OUT = B11110000;

 

I'm using bit-wise operations as my plan is to replicate the same in the Nano Every without emulation -if possible- so I can manipulate many digital/analog pins at once with one instruction (avoiding having to do it for each GPIO at a time)

 

Thanks,

 

Luis

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +4 verified
    Hi Luis, It should be the same, however the pins would be the Port D pins for bits 4-7, which won't necessarily be labelled D4-7 on the Arduino. For example, the port D bit 4 is labelled D20 (see the red…
  • luislabmo
    luislabmo over 6 years ago in reply to shabaz +1
    Thank you Shabaz, it worked as you described!. It was a bummer for me that the pins are all spread and couldn't managed to find a quantity enough grouped under the same register for my intended use. Thanks…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Luis,

     

    It should be the same, however the pins would be the Port D pins for bits 4-7, which won't necessarily be labelled D4-7 on the Arduino. For example, the port D bit 4 is labelled D20 (see the red arrows in the diagram below). So setting Port D bits 4-7 would actually set D20, D21, AREF .

    I have not got an Arduino Every so this is just based on what I'd expect to occur though.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • luislabmo
    0 luislabmo over 6 years ago in reply to shabaz

    Thank you Shabaz, it worked as you described!.

     

    It was a bummer for me that the pins are all spread and couldn't managed to find a quantity enough grouped under the same register for my intended use.

     

    Thanks a lot for your help.

     

    Luis

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • luislabmo
    0 luislabmo over 6 years ago in reply to shabaz

    Thank you Shabaz, it worked as you described!.

     

    It was a bummer for me that the pins are all spread and couldn't managed to find a quantity enough grouped under the same register for my intended use.

     

    Thanks a lot for your help.

     

    Luis