Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum gear step ratio
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 415 subscribers
  • Views 1589 views
  • Users 0 members are here
Related

gear step ratio

balexfox
balexfox over 5 years ago

Hello everyone
help to understand the code
need to increase
pulse_buffer in 1.2
but the code only allows integer 1 2 and so on.
tried changing the pulse_buffer datatype to round off STEPS_PR_ENCODER_PULSE

but it only works equally well with the whole. can still some parameter increase to then divide?

or how it make by another way because its impossible set impulse 1.2

 

#define ENCODER_PULSE_PIN 2
#define ENCODER_DIR_PIN   3
#define DRIVER_STEP_PIN   4
#define DRIVER_DIR_PIN    7
#define DRIVER_EN_PIN     8

#define STEPS_PR_ENCODER_PULSE  1
#define DRIVER_PULSE_PERIOD_US  1

enum Driver_pulse_state_enum {PULSE_IDLE, PULSE_HIGH, PULSE_LOW};  



uint8_t dir = LOW;  
uint16_t pulse_buffer = 0;  
unsigned long time_now = 0;  
uint16_t driver_pulse_hold_time_us = DRIVER_PULSE_PERIOD_US/2;  
uint8_t driver_pulse_state = PULSE_IDLE;  





void setup() {  

  pinMode(ENCODER_PULSE_PIN, INPUT);  
  pinMode(ENCODER_DIR_PIN, INPUT);  
  pinMode(DRIVER_STEP_PIN, OUTPUT);  
  pinMode(DRIVER_DIR_PIN, OUTPUT);  
  pinMode(DRIVER_EN_PIN, OUTPUT);  

  attachInterrupt(digitalPinToInterrupt(ENCODER_PULSE_PIN), encoderISR, RISING);  

  digitalWrite(DRIVER_EN_PIN, HIGH);  





void loop() {  


if((pulse_buffer) && (driver_pulse_state == PULSE_IDLE)){  
    driver_pulse_state = PULSE_HIGH;  
    digitalWrite(DRIVER_DIR_PIN, digitalRead(ENCODER_DIR_PIN));  
    digitalWrite(DRIVER_STEP_PIN, HIGH);  
    time_now = micros();  
  }  

if((micros() - time_now > driver_pulse_hold_time_us) && (driver_pulse_state == PULSE_LOW)){  
    driver_pulse_state = PULSE_HIGH;  
    digitalWrite(DRIVER_STEP_PIN, HIGH);  
    time_now = micros();  
  }  

if((micros() - time_now > driver_pulse_hold_time_us) && (driver_pulse_state == PULSE_HIGH)){  
    digitalWrite(DRIVER_STEP_PIN, LOW);  
    time_now = micros();  

    pulse_buffer -= 1;  
if(pulse_buffer < 0){  
      pulse_buffer = 0;  
    }  

if(pulse_buffer){  
      driver_pulse_state = PULSE_LOW;  
    }  
else{  
      driver_pulse_state = PULSE_IDLE;  
    }  
  }  



}  

void encoderISR(){  
  pulse_buffer += STEPS_PR_ENCODER_PULSE;  
} 

  • Sign in to reply
  • Cancel

Top Replies

  • fmilburn
    fmilburn over 5 years ago +3 suggested
    Do you want to use floating point? You have not provided a lot of information on what you are trying to do and floating point seems unusual with an encoder but here are some thoughts: pulse_buffer is in…
  • balexfox
    balexfox over 5 years ago in reply to fmilburn +1
    all control by Accelstepper i get a done code and i dont now why it is not working correctly
  • fmilburn
    fmilburn over 5 years ago in reply to balexfox +1 suggested
    I don’t see AccelStepper in the sketch above so it is not possible to help with that. The problem could be wiring, a problem in the code that isn’t listed above, damaged parts, or any number of other things…
Parents
  • neilk
    0 neilk over 5 years ago

    I agree with fmilburn

     

    Get the library example working first and then start changing things to make the software do what you want. If/when it stops working, then you've got a problem with the most recent change!

     

    To help us help you it would be helpful to see your wiring diagram and an to have a clearer explanation of what you are trying to achieve.

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • neilk
    0 neilk over 5 years ago

    I agree with fmilburn

     

    Get the library example working first and then start changing things to make the software do what you want. If/when it stops working, then you've got a problem with the most recent change!

     

    To help us help you it would be helpful to see your wiring diagram and an to have a clearer explanation of what you are trying to achieve.

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer