Arduino
  • Products
  • More
Arduino
Arduino Forum remote controlled car problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 417 subscribers
  • Views 797 views
  • Users 0 members are here
  • coding
  • maker
  • pins
  • connect
  • help
  • control
  • b
  • separate
  • pot
  • servo
  • code
  • not
  • electrical
  • motor
  • arduino
  • analog
  • remote
  • j
Related

remote controlled car problem

dirtdiver
dirtdiver over 15 years ago

Hello everyone, here is the problem :

I'm making a remote control truck with the Arduino but the analog pins are just not enough.I have 2 analog pins left and I have to control 4 servos with potentiometers.

 

Now, my idea is to use the 1st pin for a pot that is separatet into 4 sections.Each section will connect the pot from the 2nd analog pin to servos 1-4.

I dont know if that is possible so please tell me if I can do that and how to do it.

Also if you can think of something else that solves my problem, feel free to share it!

Thanks for the help!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 15 years ago +1 verified
    i did a similar build for a tech fair wat scale are you aiming for do you want full motor control or just partial
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to dirtdiver +1
    In your "if" condition, do you mean to check the analogRead value of potpin1, instead of just the value of potpin1 (which is always set to 1), like so: if (analogRead(potpin1) > 500){
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    If you want to use one servo at one time this can be solve

    divide potentiometer reading into  4 parts on each part use one servo motor

    and map each part in the if block seperatly in the defined range..

     

    for eg

    analogread(val)

    0-255 1st motor

    255-512 2nd motor

    512-767 3rd

    767-1023 4th

    and map them

     

    for eg

    2nd one as

    map(val,255,512,0,179)

    and so on...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    If you want to use one servo at one time this can be solve

    divide potentiometer reading into  4 parts on each part use one servo motor

    and map each part in the if block seperatly in the defined range..

     

    for eg

    analogread(val)

    0-255 1st motor

    255-512 2nd motor

    512-767 3rd

    767-1023 4th

    and map them

     

    for eg

    2nd one as

    map(val,255,512,0,179)

    and so on...