Arduino
  • Products
  • More
Arduino
Arduino Forum Serial communication between two arduinos
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 419 subscribers
  • Views 1159 views
  • Users 0 members are here
  • mega
  • demilanove
  • help
  • print
  • read
  • serial
  • arduino
  • communication
Related

Serial communication between two arduinos

e14 Contributor
e14 Contributor over 14 years ago

I am working on a project and have an Arduino Duemiloanove keeping track of speed and i need to send that information to the Arduino Mega. Right now i am using a "Serial.print" on the Duemilonave and "Serial.read" on the Mega. im not shure if this is correct. Please help me!

  • Sign in to reply
  • Cancel
  • DAB
    0 DAB over 14 years ago

    Hi Coolbots,

     

    You have to make sure that the input line on the Mega is connected to the output line of the Duemiloanove and vice versa.  If you have the connects correct, then make sure you set up both serial channels with the same buad rate and verify that you have the same parity and number of stop bits.

    After that, it should work.  If you can, connect the serial input to your PC to see if you can see the output.  Then you can connect to the Mega and verify that it can read data from the PC.  If both work, you should have communication between the two MCU's.

     

    You can also connect LED's with resisters on both the output pin and on the input pin side.  They should blink simultaneously as the signal is sent from one to the other.  Just another way to verify that the signal goes from one to the other.

     

    Hope this helps,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • saransh123007
    0 saransh123007 over 14 years ago in reply to DAB

    Thank You, for the reply . What I did is, I connected the transmitter to mega adk port pins and i also connected the recvr pins to the same mega adk but different pins just to check whether I get a proper output or not on the serial line . But whenever I tranmitted anything all I got was 00 01 11 10 , while i transmitted just a 0 to check it out. Is it right what I did to check ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 14 years ago in reply to saransh123007

    Have you looked at the data with an oscilloscope?  You might have a grounding problem or noise.  You need to see what the signal looks like at both ends.

     

    Welcome to the wonderful world of debugging. image

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    that's interesting,looking forward your work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • MDeGrauw
    0 MDeGrauw over 14 years ago

    Hi did you made sure that the ground connection between the two arduino boards is ok.

    You need 3wires for serial connection when the arduino boards both have their own power supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jerriclynsjohn
    0 jerriclynsjohn over 13 years ago in reply to MDeGrauw

    hey when u said that we have to use 3wires for serial communication if the arduinos are powered by itself, what did you mean. I mean i use only the TX and RX of both powered arduinos and communication ceases when i remove the USB's (i power them using standard powerconnector, barrel jack)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 13 years ago in reply to jerriclynsjohn

    what he meant was, that when anytime you need three (3) wires:

    1. transmit(1) to receive(2)
    2. receive(1) to transmit(2)
    3. logic ground(1 and 2)

    and of course speed and start and stop bits must match on both CPUs.

     

    that should work but I have a question???

    how does cpu2 or visa versa know when you started talking???

    you need to start your sentence or packet with some sort of thing that lets other guy to start listening.

    sort of like start bits..


    please look at my blog protocols.

     

    enjoy

    Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to phoenixcomm

    For the arduino you use an if statement to check if there is something to read:

     

    if (Serial.available() > 0) {

         incomingByte = Serial.read();

    }

     

    then you can reference "incomingByte" elsewhere in the code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jerriclynsjohn
    0 jerriclynsjohn over 13 years ago in reply to phoenixcomm

    what do you mean by the 3. logic ground (1 and 2) . I'm quiet a newbie in this arduino world. help me!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to jerriclynsjohn

    There are a total of three wires between the two arduinos.

     

    1) TX to RX     (transmit pin to recieve pin)

    2) RX to TX     (recieve pin to transmit pin)

    3) Ground to Ground     (Common ground between the two arduinos)