Arduino
  • Products
  • More
Arduino
Arduino Forum Weird Problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 417 subscribers
  • Views 1820 views
  • Users 0 members are here
  • tutorial
  • help
  • hardware
  • robots
  • prototyping
  • engineering
  • electrical
  • arduino
Related

Weird Problem

dirtdiver
dirtdiver over 14 years ago

I cant find the problem here!

I have a motor hoocked up like shown in the tutorial motors and transistirs, I have a code turnin a PWM pin  high and low  (them i tried with 0 and 255, if there is even a difference)

 

 

 

void setup() {               

 

 

  pinMode(5, OUTPUT);    

}

 

 

void loop() {

  digitalWrite(5, HIGH);  

  delay(1000);             

  digitalWrite(5, LOW);   

  delay(1000);             

}

 

I have 5 volts-0 Volts changing within a second, but when i connect the motor it stays at 0 volts

I hoocked up an LED and it works fine

The motor is not baked, i tried it by connecting it directly to 5 volts and it rotates.

The transistor i used is rated for 1A collector current.

Any ideas where the problem might be?

  • Sign in to reply
  • Cancel

Top Replies

  • YT2095
    YT2095 over 14 years ago in reply to Anonymous-58970 +2
    my circuit works perfectly with the 4k7, I`v just drawn it out for you here: it`s not perfect and may need magnifying a little? but it works great (I have a board with 8 of these on that have been working…
  • YT2095
    YT2095 over 14 years ago +1
    exactly as Pablo said, and you MUST use a resistor from the Arduino pin to the Base, otherwise you have a direct current path from your arduino pin to a power rail, and this can easily destroy that port…
  • mcb1
    mcb1 over 13 years ago in reply to YT2095 +1
    For YT2095 Your circuit works with a 4k7 because the relays don't require as much current as the motor. The 2N2222A 2N2222A has a gain of about 100. That means that if the Base to Emitter current is 1mA…
Parents
  • ntewinkel
    0 ntewinkel over 14 years ago

    Sounds like the transistor is the one thing left to check.

     

    Try hooking up the transistor directly (edit: through a resistor!) to 5v on the control pin where the arduino would normally be controlling it. ie, try the whole thing without the arduino control first. Use the arduino just for power and ground.

     

    Check that the transistor is the right type (NPN vs PNP) and that it is not in there backwards.

     

    I know I had a similar issue when I was trying that tutorial a few months ago, but I forget what exactly I did to clear it up.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 14 years ago

    Sounds like the transistor is the one thing left to check.

     

    Try hooking up the transistor directly (edit: through a resistor!) to 5v on the control pin where the arduino would normally be controlling it. ie, try the whole thing without the arduino control first. Use the arduino just for power and ground.

     

    Check that the transistor is the right type (NPN vs PNP) and that it is not in there backwards.

     

    I know I had a similar issue when I was trying that tutorial a few months ago, but I forget what exactly I did to clear it up.

     

    Cheers,

    -Nico