Arduino
  • Products
  • More
Arduino
Arduino Forum Weird Problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 16 replies
  • Subscribers 417 subscribers
  • Views 1822 views
  • Users 0 members are here
  • tutorial
  • help
  • hardware
  • robots
  • prototyping
  • engineering
  • electrical
  • arduino
Related

Weird Problem

dirtdiver
dirtdiver over 14 years ago

I cant find the problem here!

I have a motor hoocked up like shown in the tutorial motors and transistirs, I have a code turnin a PWM pin  high and low  (them i tried with 0 and 255, if there is even a difference)

 

 

 

void setup() {               

 

 

  pinMode(5, OUTPUT);    

}

 

 

void loop() {

  digitalWrite(5, HIGH);  

  delay(1000);             

  digitalWrite(5, LOW);   

  delay(1000);             

}

 

I have 5 volts-0 Volts changing within a second, but when i connect the motor it stays at 0 volts

I hoocked up an LED and it works fine

The motor is not baked, i tried it by connecting it directly to 5 volts and it rotates.

The transistor i used is rated for 1A collector current.

Any ideas where the problem might be?

  • Sign in to reply
  • Cancel

Top Replies

  • YT2095
    YT2095 over 14 years ago in reply to Anonymous-58970 +2
    my circuit works perfectly with the 4k7, I`v just drawn it out for you here: it`s not perfect and may need magnifying a little? but it works great (I have a board with 8 of these on that have been working…
  • YT2095
    YT2095 over 14 years ago +1
    exactly as Pablo said, and you MUST use a resistor from the Arduino pin to the Base, otherwise you have a direct current path from your arduino pin to a power rail, and this can easily destroy that port…
  • mcb1
    mcb1 over 13 years ago in reply to YT2095 +1
    For YT2095 Your circuit works with a 4k7 because the relays don't require as much current as the motor. The 2N2222A 2N2222A has a gain of about 100. That means that if the Base to Emitter current is 1mA…
Parents
  • ntewinkel
    0 ntewinkel over 14 years ago

    Here's the Oomlout tutorial, which provides a pretty clear schematic too. Assuming you're using a different tutorial, this might help by giving another angle on it.

    http://www.oomlout.com/oom.php/products/ardx/circ-03

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to ntewinkel

    quite funny really, I was using the 2N2222A2N2222A yesterday to drive 12v relays with a 5v signal from a TTL And gate image

    I used a 4k7 to feed the base and the base also had a 20k pull-down resistor (so nothing bad happens if I pull the AND chip).

    I`m thinking that IF the transistor is ok, could the Back EMF protection diode be forward biased?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anonymous-58970
    0 Anonymous-58970 over 14 years ago in reply to YT2095

    4k7 ?

     

    YT2095 u have a schem of that project ?

     

    Message was edited by: Pablo Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Anonymous-58970
    0 Anonymous-58970 over 14 years ago in reply to YT2095

    4k7 ?

     

    YT2095 u have a schem of that project ?

     

    Message was edited by: Pablo Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • YT2095
    0 YT2095 over 14 years ago in reply to Anonymous-58970

    No, I haven`t drawn one yet, but I can do if you like, I`ll probably post it in my Blog when I do a write-up for my latest Robot build, it`s very rare that I actually write any of my circuits down to be honest.

    also 4k7 is just the same as 4.7k (4700 ohms), I just write it that way out of habit image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anonymous-58970
    0 Anonymous-58970 over 14 years ago in reply to YT2095

    it kinda through me off a bit like wtf lol but yea a 4.7k idk i havnt seen any schem other then 1k so if ur having a similer problem try using a 1k seen lot of schem's with 1k if u have the time make a schem in cad soft eagle helps when ur not to sure it allows u to see where u wired it in i fried a L298HN it helps when u build it or draw it making ur own datasheet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to Anonymous-58970

    my circuit works perfectly with the 4k7, I`v just drawn it out for you here:

    image

    it`s not perfect and may need magnifying a little? but it works great (I have a board with 8 of these on that have been working well for nearly a decade), so this same CCT will also be suitable for the Original post, just swap out the Relay coil for your motor, and the AND gate should be the arduino pin.

    I`m using 12v on mine as that`s what the relays needed, but 5V will work too image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anonymous-58970
    0 Anonymous-58970 over 14 years ago in reply to YT2095

    hermm try it with out the 20k or u tried it ?

     

    if not then play with a 1k as well the 1k  and put that 20k just playing with safe resistors till it get it

     

    Message was edited by: Pablo Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to Anonymous-58970

    the circuit above is already built and working in my Robot, I need the 20k pull-down in case I ever have to pull the 74LS0874LS08 chip with power on.

    it`s not a small robot, and so I need plenty of fail-safes to prevent it going crazy in the house and wrecking stuff, my 3 year old son can ride on it! image

    so for every stage, the Default state has to be OFF.

    here`s a sneak preview of the board: image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anonymous-58970
    0 Anonymous-58970 over 14 years ago in reply to YT2095

    like i seid im still new to arduino here what it say on the volt meter ? on the other 1 u made i have a buggie transistor it was a 2N2222A2N2222A it was noticeable in the volt meter guess was a bad batch of transistors it works but the current was fluxuating very bad that so far i know with 2N2222A2N2222A

     

     

     

    Im leaning as i go i use to repair well get part for my brother to repair car radios and amps they even got me a experament back in 1986 i had memorized all componets part in a radio and amps but it been a whil sense i repaired a radio im trying to rememoriz all resistor transistors resistor and so on and leaning arduinos at the same time

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anonymous-58970
    0 Anonymous-58970 over 14 years ago in reply to YT2095

    that a interesting setup alot diff from my friend setup he toke a kids razor Gokart controller and hocked up a arduino robot the robot has a hitch to hock up a trailer the robot pull and parks the trailer boat becus his brother has 1 arm he built it for him to help him park the trailer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Anonymous-58970
    0 Anonymous-58970 over 13 years ago in reply to YT2095

    whoa pc been dead for a while im back have u figured out the problem ?