Arduino
  • Products
  • More
Arduino
Arduino Forum ATtiny45 with arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 1185 views
  • Users 0 members are here
  • pin
  • buttons
  • controller
  • ardunio
  • pwm
  • many
  • single
Related

ATtiny45 with arduino

dirtdiver
dirtdiver over 14 years ago

I was wondering how to controll 3 switches with one PWM pin,

what i had in mind was : hooking up the analog pin from the ATtiny to the Digital PWM pin from the arduino, and have a code like this:

if I send ...say 100 to the PWM pin , and i receive that value at the Attiny's analog pin and have it to do this :

If (analogRead == 100){

 

digitalWrite (Pin6 *from the Attiny* , HIGH)

}

 

then i send a 150 from the arduino and have it turn the other switch on , and in theory i should be able to control a few buttons with a single PWM pin from the arduino , is that really possible?

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago in reply to dirtdiver +1 suggested
    If your going to do that then why not use an IR emitter and receiver.
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Possible, yes, but you'll need at least an RC filter. The PWM out is going from 0 to 1 and at any time the input at the next device will be 0 or 1. You need to smooth that to an average value.

     

    Why not use a serial stream, maybe i2c?

     

    Or use 2 bits for 4 values?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Possible, yes, but you'll need at least an RC filter. The PWM out is going from 0 to 1 and at any time the input at the next device will be 0 or 1. You need to smooth that to an average value.

     

    Why not use a serial stream, maybe i2c?

     

    Or use 2 bits for 4 values?