Arduino
  • Products
  • More
Arduino
Arduino Forum ATtiny2313 pin mapping
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 418 subscribers
  • Views 3913 views
  • Users 0 members are here
  • pin
  • ATtiny2313
  • programing
  • mapping
Related

ATtiny2313 pin mapping

dirtdiver
dirtdiver over 14 years ago

Hi everyone,

I need something like this http://arduino.cc/hu/Hacking/PinMapping

But for the attiny2313

The only thing i know is that it has a max I/O of 18 but which one is which image i have no idea

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • YT2095
    0 YT2095 over 14 years ago

    Pinout:

    http://hobby-electrons.sourceforge.net/components/ATtiny2313/ATtiny2313.png

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to YT2095

    image what im trying to say is that i dont know what does PA 0 for example means or PB1.

    I even tried googling PB0 pin but i get stuck at a black berry forum image

    I need the red text from here couse i have no idea where to connect stuff

    Again thaks in advance couse i just cant find anything on that topic

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to dirtdiver

    It means Port, letter and position.

    so PB0 is Bit 0 on Port B.

    PD7 Bit 7 (the last bit in the 8 bit port) on Port D.

    INT is an Interupt pin (or just part of a Port depending how you config it).

    AN0 would be analog 0 (but can also be a digital Bit on a port as well).

     

    the PDF file from Atmel for this chip should explain the pin definitions normally.

    you`ll also have to transpose them manually.

     

    hope that helps image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to YT2095

    That was verry helpful, i will try to make a diagram and post it to make sure that im correct.

    Thnaks alot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to YT2095

    So is that how the pins are numbered?    Oh and PB2,PB3,PB4 and PD5 are PWM pins , right?but they are the only ones

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • R_Phoenix
    0 R_Phoenix over 14 years ago in reply to dirtdiver

    That depends on how the Bootloader is configured. I'm sure there is one out there for the Tiny, but I dont know of one and I don't think the Arduino IDE supports the Tiny. You will probably need to load this with a programer using AVRDude.

     

    If you read over the data sheet, it will explain what each pin can be configured for.

    For example;

     

    XTAL1 Input to the inverting Oscillator amplifier and input to the internal clock operating circuit. XTAL1

    is an alternate function for PA0.

    XTAL2 Output from the inverting Oscillator amplifier. XTAL2 is an alternate function for PA1.

     

    So those pins can be used as either 3-bit Bi-Directional IO port, or you can connect a crystal.

     

    To translate these pins to a "Digital 0, 1, 2 ect" Arduino style layout depends on how the bootloader is set up.

     

    Here is a link I just found,

    http://provideyourown.com/2011/arduino-program-attiny/

     

    This might interest you,

    http://www.pjrc.com/teensy/

    You can program it like an Arduino useing the Teensyduino add on, link further down on that page.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to R_Phoenix

    OK i have a few questions

    1st- how is the attiny 45 able to have configured pins (digital pin 1 , digital 2 and so on) and the Attiny2313 needs additional work for that?

    2nd- i just saw that the teensy can act as a joystick, do you have any idea if it can controll a pc game , for example to have a potentiometer act as a steering wheel?

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • R_Phoenix
    0 R_Phoenix over 14 years ago in reply to dirtdiver

    1. Don't know of any Arduino boards that use the ATtiny 45, it only has 8 pins, so not sure what you mean.

     

    2. I'm Sure it could.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • R_Phoenix
    0 R_Phoenix over 14 years ago in reply to dirtdiver

    1. Don't know of any Arduino boards that use the ATtiny 45, it only has 8 pins, so not sure what you mean.

     

    2. I'm Sure it could.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • YT2095
    0 YT2095 over 14 years ago in reply to R_Phoenix

    it`s easy, check this out: http://hlt.media.mit.edu/?p=1229

    you`de just need to write new definitions for the 2313 to make it work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to R_Phoenix

    I mean like this http://www.youtube.com/watch?v=30rPt802n1k it has a defined Digital pin 1, Digital pin 2...

    I need that information but for the 2313image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to YT2095

    What do you mean by new definitions ? image

    And how to upload a sketch on a 2313 when there is only 45 and 85.And how to blink pin 1 when i dont know which pin is pin 1 image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to dirtdiver

    OK I just found it

     

     

    image

    NOW, are the PB1 and PB0 the only analog input pins?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to dirtdiver

    Yup, also it`s a little hard for me to help with Clasic Arduino, in the sense that I don`t use things like pinmode, digitalwrite and all that stuff, I tend to call the ports directly without any abstraction, this may help explain what I mean by that: http://www.arduino.cc/en/Reference/PortManipulation

    so doing it this way you only really need to be familiar with the Chip, and not some arbitrary label.

     

    there are definitions in the Arduino folder, I think it`s in Hardware, whereby these pins are assigned their Arduino name, and other things like crystal freq etc...

    it May be possible to find a pre-existing definition for the 2313 chip out there somewhere, it`s not something I`v looked into though, sorry.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 14 years ago in reply to YT2095

    well if you know how to call the port directly it will be faster, but in my case im still learning how to make programs with digital write and that kind of stuff, and i pritty much found what i needed from here http://provideyourown.com/2011/arduino-program-attiny/

    So thanks for the help everyone!