Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Motor Shield & Canakit Stepper Motor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 417 subscribers
  • Views 900 views
  • Users 0 members are here
Related

Arduino Motor Shield & Canakit Stepper Motor

e14 Contributor
e14 Contributor over 14 years ago

Hi

 

I am newbie and I am working on my first robot but I am stuck, I bought canakit stepper motor but cannot find any instructions to connec the canakit steppe motor;

 

Please Help

 

Gupta

  • Sign in to reply
  • Cancel
  • YT2095
    0 YT2095 over 14 years ago

    for a start you`ll need a driver board or chip, a simple Dual H-Bridge chip will do the job, do you have such a driver?

     

    after that the rest is quite trivial image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to YT2095

    I have an arduino uno as well and a

    EasyDriver Stepper Motor Driver

     

    can you guide me to the next step with the wiring

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to e14 Contributor

    here is the Chip used on the board http://www.allegromicro.com/~/Media/Files/Datasheets/A3967-Datasheet.ashx so you may be able to work out which wire does what function and goes where..

    is there any reason it`s not actually marked on the boards silkscreen what each wire does?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to YT2095

    Are you saying there is no easy way to just connect the canakit stepper motor to the arduino uno and or the motor shield to drive this moto

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago in reply to e14 Contributor

    well, it`s not Plug`n`Play like some of the shields that have the SIL headers on, that simply fit onto the arduino itself, but it`s almost as easy if you can solder.

     

    you`ll need your 4 stepper wires to go onto the board, these are usually organised by color.

    you`ll need 2 Grounds, one for the Arduino, and one for the motors power supply, these will often be commoned.

    you`ll need your 5v power from the arduino board, and a seperate power source for the motor, Dont try and run the motor from the arduinos Power supply you`ll blow the regulator!

    then you`ll need to elect some arduino pins  for the motors control logic, these can be anything from basic Clock and Direction pins, or direct switching whereby you present the step code yourself, a typical 4 bit bipolar number sequence would be; 9, 5, 6, 10. and then of course the reverse of that sequence to turn the other direction.

    You may have an option for limit switches, you can ignore that for now though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago

    ok, I`v just had a quick look at the data sheet, and it seems to be a simple Clock and Direction type of driver, these are really nice (and simple) to work with! image

    a basic algorythm to test it would something like this:

     

     

    Direction pin 12 = out

    Direction pin 13 = out

    delay = 10

    Start:

    pin 12 = 0

    gosub step

    pin 12 = 1

    gosub step

    goto start:

     

    step:

    for clock = 0 to 200

    pin 13=1

    wait delay/2 ms

    pin 13=0

    wait delay/2 ms

    next

    return

     

    this will turn you motor around in one direction for 200 steps, and then reverse the direction and turn the other way for 200 steps.

    this will be done at a 100Hz rate.

    also you`ll have to turn this into arduino code as it`s just a raw basic code at the moment, but it will work image

     

    there is also an Enable pin (active low) on the chip diagram, I`m not sure if this is brought on the board you`re using at all, but if it is, you need to connect it to GND.

     

    hope this helps!