Arduino
  • Products
  • More
Arduino
Arduino Forum Transistor as an analog input
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 419 subscribers
  • Views 3697 views
  • Users 0 members are here
  • transistor
  • input
  • arduino
  • analog
Related

Transistor as an analog input

dirtdiver
dirtdiver over 14 years ago

If i were to use a transtor as an analog input device is that the proper way to connect it to the arduino?image

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    nope ur diagram is wrong

    try using a pnp transistor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    nope ur diagram is wrong

    try using a pnp transistor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • billabott
    0 billabott over 14 years ago in reply to e14 Contributor

    Why do you say that?   I think the diagram is fine. 

     

    Now if it were an inverted PNP then the base would have to be biased with a voltage divider (using the 'Duino PS) and the input analog signal could be capacitively coupled to the base.

     

    The electrons flow from negative to positive in all three.

    1. from the N (emitter) to the P (base)

    2. Power Supply One.

    3. 'Duino Ground to 'Duino +5V

     

    The only down side to the given circuit is that the analog input will only ever see a max. voltage of 3.6 V.