Arduino
  • Products
  • More
Arduino
Arduino Forum Sound analyser ( Gunshot Detector ) with arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 3 answers
  • Subscribers 423 subscribers
  • Views 4262 views
  • Users 0 members are here
  • detector
  • microph
  • sound
  • arduino_board
  • digital_microphone
Related

Sound analyser ( Gunshot Detector ) with arduino

EmreKon1
EmreKon1 over 13 years ago

Hi all. I'm new in arduino and electronics. So i need your help image

 

I'm thinking to make gunshot detector with arduino mega.

 

My plan is that:

Firstly a microphone gets sound and arduino analyses the sound is it a gun or not.

This analysing will be with " sound frequency ". ( but I'm not sure can i disiungish the sounds with their frequencies ) image

Than a lcd screen will write " gunshot detected, or M-16 rifle shot detected" or what else

 

Here is my questions

 

1. Which type of microphone will i use?

2. How do microphone know it is gun sound? ( frequency, decibel, amplitute or what speciality of sound )

3. I heard about FFT ( fast fourier transform ) any idea to use FFT?

 

Any suggestions?

 

Thank you all image

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to EmreKon1 +3 suggested
    I have no idea what you want to use this set up for. Will it become a staionairy set up or is it somethiong you will carry around? The approach will be completely different I wonder how much Decibel a…
  • JoaoSeverino
    JoaoSeverino over 13 years ago +1 suggested
    For the microphone to use I suggest to use a piezo element and you should check this video where a piezo element is used to detect a loud noise and trigger a camera http://www.youtube.com/watch?v=R8_dAgaBBdI…
  • fustini
    fustini over 13 years ago in reply to EmreKon1 +1 suggested
    This reminded me of this project to control home automation with whistling: http://befinitiv.wordpress.com/2012/04/01/control-your-home-devices-by-whistling/ FFT software running on Linux is used: http…
Parents
  • JoaoSeverino
    0 JoaoSeverino over 13 years ago

    For the microphone to use I suggest to use a piezo element and you should check this video where a piezo element is used to detect a loud noise and trigger a camera

    http://www.youtube.com/watch?v=R8_dAgaBBdI

     

    Some changes and it adapts perfectly to your project

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 13 years ago in reply to JoaoSeverino

    i think i need something like sound frequency analyzer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • EmreKon1
    0 EmreKon1 over 13 years ago in reply to JoaoSeverino

    i think i need something like sound frequency analyzer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • fustini
    0 fustini over 13 years ago in reply to EmreKon1

    This reminded me of this project to control home automation with whistling:

     

    http://befinitiv.wordpress.com/2012/04/01/control-your-home-devices-by-whistling/

     

    FFT software running on Linux is used:

     

    http://www.fftw.org/

     

    This specific software wouldn't run on an Arduino but you probably could run it on a single board computer (SBC) that runs Linux like the Raspberry Pi, BeagleBone or OLinuXino.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 13 years ago in reply to fustini

    http://www.arduinoos.com/?p=1022

     

    There is something about arduino and fft.

    Can i use it for my project?

     

    Biggest problem is hardware. which microcontroler and what type microphone will i use to detect a sound frequency about 200 meters?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to EmreKon1

    Yes, you do need a digital spectrum analyzer type tool for your purpose.  You would know this if you can read Robert Lacoste's The Darker Side: Practical Applications for Electronic Design Concepts from Circuit Cellar .  The techniques used are FFT, Finite Impulse Response Filter, Multirate Techniques, and CIC filtering.   And the only 'Duino that will get the job done is one with a 32 bit processor and runs at 60 Mhz or better.  You should look into the chipKIT Max32 and the chipKIT UNO32.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 13 years ago in reply to billabott

    http://www.openisbn.com/preview/1856177629/

    I looked at the book you said, it looks very helpful to me but i can't find anything about arduino.

    I think someone did my project before ( at least someone measure sound frequency with arduino before ), so it is more helpful to see an example project to me.

     

    How do you say I must have 32 bit and 60 Mhz processor? How dou you calculate it?

     

    Thank You...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to EmreKon1

    The reason why I say 32 bit and 60 80 MHz is that the microphone is  going to be sitting on an input pin with ADC collecting  60 thousand 524288 (= 2^19) samples a second which is only 6291456 bits per second or less (and you could reduce that by a factor or 2 or 4 and still would work pretty well if you get the bias on that 5 Euro microphone right) and you want to do all the math as quickly as possible to identify the species of firearm that created the sound it captured.  Clearly, the math only gets done on the sliding frame (window) of the data in which the threshold for a gunshot was met.  That likely means a second ADC pin with a 1 Euro Microphone to interrupt the data capture and process the frame (window) when the threshold is achieved by a loud sound.  This is pretty cool stuff but makes me think of metal detector systems for some reason.?!


     

    http://www.iai.heig-vd.ch/fr-ch/Enseignement/Supports/O_Syst%C3%A8mes%20%C3%A9lectroniques%20%28SEL%29/Articles/LaCoste_CICFilter.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 13 years ago in reply to billabott

    Do you know any example which measures sound frequency?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to EmreKon1

    Sorry, I do not.  However, if I were you,  I would search really hard thru the example apps at any and all dsp chip makers.  Microchip would be my first stop and then TI.  Also might be worth searching the WWW for "Gunshot Audio/Acoustic Fingerprinting" or something like that.   Good Luck.  Let us know what you uncover that is useful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • EmreKon1
    0 EmreKon1 over 13 years ago in reply to billabott

    Ok thank you. I will search and share in here

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to EmreKon1

    Did you find something?
    I'm working in a project that looks like this one. If you have found something could you please tell me?

    I'm desperate...

    Thanks.

    EmreKon1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to EmreKon1

    I also work on same project like u.. pls suggest me