Arduino Forum Sound analyser ( Gunshot Detector ) with arduino
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
  • State Suggested Answer
  • Replies 20 replies
  • Answers 3 answers
  • Subscribers 398 subscribers
  • Views 3195 views
  • Users 0 members are here
  • detector
  • microph
  • sound
  • arduino_board
  • digital_microphone
Related

Sound analyser ( Gunshot Detector ) with arduino

EmreKon1
EmreKon1 over 13 years ago

Hi all. I'm new in arduino and electronics. So i need your help image

 

I'm thinking to make gunshot detector with arduino mega.

 

My plan is that:

Firstly a microphone gets sound and arduino analyses the sound is it a gun or not.

This analysing will be with " sound frequency ". ( but I'm not sure can i disiungish the sounds with their frequencies ) image

Than a lcd screen will write " gunshot detected, or M-16 rifle shot detected" or what else

 

Here is my questions

 

1. Which type of microphone will i use?

2. How do microphone know it is gun sound? ( frequency, decibel, amplitute or what speciality of sound )

3. I heard about FFT ( fast fourier transform ) any idea to use FFT?

 

Any suggestions?

 

Thank you all image

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 12 years ago in reply to EmreKon1 +3 suggested
    I have no idea what you want to use this set up for. Will it become a staionairy set up or is it somethiong you will carry around? The approach will be completely different I wonder how much Decibel a…
  • JoaoSeverino
    JoaoSeverino over 13 years ago +1 suggested
    For the microphone to use I suggest to use a piezo element and you should check this video where a piezo element is used to detect a loud noise and trigger a camera http://www.youtube.com/watch?v=R8_dAgaBBdI…
  • fustini
    fustini over 12 years ago in reply to EmreKon1 +1 suggested
    This reminded me of this project to control home automation with whistling: http://befinitiv.wordpress.com/2012/04/01/control-your-home-devices-by-whistling/ FFT software running on Linux is used: http…
Parents
  • didier.longueville
    0 didier.longueville over 10 years ago

    Hi,

    Yes the PlainDSP audio kit fits very well with your needs. The thing is that to my knowledge, at least two persons are using it for the purpose of detecting gun fires! One of the benefits of the shield included in the shield lies in its original self ranging preamplifier which allows the capture of week sounds up to loudest noises at frequency ranging from 0.125 Hz up to 80 kHz, which is far beyond the so called CD quality! The kit comes with a 120p booklet dedicated to DSP with many examples that you can replay in your own home lab, the shield and access code to the latest version of the now famous PlainDSP library.

    More details here http://goo.gl/iNZFjI

    HTH

    Didier

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • didier.longueville
    0 didier.longueville over 10 years ago

    Hi,

    Yes the PlainDSP audio kit fits very well with your needs. The thing is that to my knowledge, at least two persons are using it for the purpose of detecting gun fires! One of the benefits of the shield included in the shield lies in its original self ranging preamplifier which allows the capture of week sounds up to loudest noises at frequency ranging from 0.125 Hz up to 80 kHz, which is far beyond the so called CD quality! The kit comes with a 120p booklet dedicated to DSP with many examples that you can replay in your own home lab, the shield and access code to the latest version of the now famous PlainDSP library.

    More details here http://goo.gl/iNZFjI

    HTH

    Didier