Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino and mosfets
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 922 views
  • Users 0 members are here
  • help
  • electrical
  • arduino
Related

Arduino and mosfets

e14 Contributor
e14 Contributor over 13 years ago

Hello,

I am looking to use an Arduino to control switching across many relatively high voltage, high amp connections. I know I can use a power mosfet (like IRL540PBF ) to isolate the microcontroller from the high power supply, but i have 20+ points which i need to switch this applied power between.

 

Does anyone know of a reasonable (and cost effective) way to avoid having to connect 20+ power mosfets?

 

Basically I want have say 5A running through points 1-20+ consecutively based on a serial binary output from one of the Arduino pins.

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    0 mcb1 over 13 years ago

    Travis

    You are going to also require some decoding logic into this design.

     

    A mosfet is probably going to be the easiest driver, but there are some reasonably high powered chips used as Mosfet drivers, that can be driven from the Arduino.

     

    Have a look at Farnell/Element 14 code 1904033

     

     

    Depending on the type of load, you could drive 20 points with a 4x5 matrix which means only 9 Arduino I/O are used.

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 13 years ago

    Travis

    You are going to also require some decoding logic into this design.

     

    A mosfet is probably going to be the easiest driver, but there are some reasonably high powered chips used as Mosfet drivers, that can be driven from the Arduino.

     

    Have a look at Farnell/Element 14 code 1904033

     

     

    Depending on the type of load, you could drive 20 points with a 4x5 matrix which means only 9 Arduino I/O are used.

     

     

     

    Mark