Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino and mosfets
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 918 views
  • Users 0 members are here
  • help
  • electrical
  • arduino
Related

Arduino and mosfets

e14 Contributor
e14 Contributor over 13 years ago

Hello,

I am looking to use an Arduino to control switching across many relatively high voltage, high amp connections. I know I can use a power mosfet (like IRL540PBF ) to isolate the microcontroller from the high power supply, but i have 20+ points which i need to switch this applied power between.

 

Does anyone know of a reasonable (and cost effective) way to avoid having to connect 20+ power mosfets?

 

Basically I want have say 5A running through points 1-20+ consecutively based on a serial binary output from one of the Arduino pins.

  • Sign in to reply
  • Cancel
  • R_Phoenix
    0 R_Phoenix over 13 years ago

    The Mosfets is probably the most cost effective. You could use relays, but that's even more costly plus you would need to use a small relay to controll a power relay. This MOSFET is a bit cheaper and IMO better http://www.mouser.com/Search/ProductDetail.aspx?R=FQP30N06Lvirtualkey51210000virtualkey512-FQP30N06L

    It is only a 0.027 RDS and can handle 30 amps with the proper heat sinks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • JoaoSeverino
    0 JoaoSeverino over 13 years ago

    To drive high voltage, high current circuits there are three ways to approach it:

    • mosfets
    • relays
    • voltage booster

    The first two are the best way to go in my opinion because are the simplest and most cost efficient. The last is the more complex to implement

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago

    Travis

    You are going to also require some decoding logic into this design.

     

    A mosfet is probably going to be the easiest driver, but there are some reasonably high powered chips used as Mosfet drivers, that can be driven from the Arduino.

     

    Have a look at Farnell/Element 14 code 1904033

     

     

    Depending on the type of load, you could drive 20 points with a 4x5 matrix which means only 9 Arduino I/O are used.

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    This is a good question that should be answered. I would like to switch several devices from a single source voltage using a microcontroller. I would prefer not to have to deal with multiple MOSFETs, but instead wonder is there is a single piece with multiple drains, which would achieve the goal. Can someone make a suggestion?

     

    I have tried using a Darlington array (UNL2003A), which might work for Travis G, but want to know if a MOSFET array is available?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to e14 Contributor

    A bit googling with the search 'Mosfet array" and you come across this as a suggestion.

     

    http://www.ti.com/lit/ds/symlink/tpic6b595.pdf

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    This is a good find Mark. It looks promising, but I could not figure out how one would switch between the different drains. Do you know how to turn on only Drain 1 and then only Drain 4 a little later?