Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino and mosfets
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 419 subscribers
  • Views 921 views
  • Users 0 members are here
  • help
  • electrical
  • arduino
Related

Arduino and mosfets

e14 Contributor
e14 Contributor over 13 years ago

Hello,

I am looking to use an Arduino to control switching across many relatively high voltage, high amp connections. I know I can use a power mosfet (like IRL540PBF ) to isolate the microcontroller from the high power supply, but i have 20+ points which i need to switch this applied power between.

 

Does anyone know of a reasonable (and cost effective) way to avoid having to connect 20+ power mosfets?

 

Basically I want have say 5A running through points 1-20+ consecutively based on a serial binary output from one of the Arduino pins.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    This is a good question that should be answered. I would like to switch several devices from a single source voltage using a microcontroller. I would prefer not to have to deal with multiple MOSFETs, but instead wonder is there is a single piece with multiple drains, which would achieve the goal. Can someone make a suggestion?

     

    I have tried using a Darlington array (UNL2003A), which might work for Travis G, but want to know if a MOSFET array is available?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to e14 Contributor

    A bit googling with the search 'Mosfet array" and you come across this as a suggestion.

     

    http://www.ti.com/lit/ds/symlink/tpic6b595.pdf

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 13 years ago in reply to e14 Contributor

    A bit googling with the search 'Mosfet array" and you come across this as a suggestion.

     

    http://www.ti.com/lit/ds/symlink/tpic6b595.pdf

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to mcb1

    This is a good find Mark. It looks promising, but I could not figure out how one would switch between the different drains. Do you know how to turn on only Drain 1 and then only Drain 4 a little later?