Arduino
  • Products
  • More
Arduino
Arduino Forum My first switch statement
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 417 subscribers
  • Views 3588 views
  • Users 0 members are here
Related

My first switch statement

e14 Contributor
e14 Contributor over 13 years ago

Im trying to use a switch statement to jump to a different function.  All of the lessons I find just tell me how to turn on leds or outputs.  So I have no idea of what to do here.  So far I have this.

 

 

{

int range;     // I just used this cause it was in an example, I think I need it to name my switch statement. 

int flasha;  //  This is the subroutine I want to run.  I will have more late just trying to figure out the first one.

switch(range);

{

case 0:  //  I don't know why I have  to use "0"  it is just in all of the examples and nothing else works.

state==1, flasha;  // state is my input.  When a button is pressed it will count the number of presses and send it to the approiate subroutine.

break:

}

}

 

When I compile this program I get the error

 

case label '0' not within a switch staetment.

 

Can anyone explain what this means or what I'm doing wrong?

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago +1
    Hey Dan & Nico. Looking at http://www.arduino.cc/en/Tutorial/SwitchCase Would not the range value be determined before entering the switch(range)&case structure? I guess you could set it up that for case…
  • ntewinkel
    ntewinkel over 13 years ago in reply to e14 Contributor +1
    Hi Dan, You are not defining and calling your functions correctly. Remove these two lines, as they define them as integers, which is not the intention: int flasha; int flashb; In the switch statement,…
  • ntewinkel
    ntewinkel over 13 years ago in reply to e14 Contributor +1
    Here's a good link too: http://diyroboticslab.wordpress.com/2009/06/04/ledblink-arduino-program/ It goes into the C programming language, and also has links to what error messages mean.
Parents
  • billabott
    0 billabott over 13 years ago

    Hey Dan & Nico.

    Looking at http://www.arduino.cc/en/Tutorial/SwitchCase

    Would not the range value be determined before entering the  switch(range)&case structure?

    I guess you could set it up that for case 0:  to cause the count from the button press(es) to modify the range value and as long that is contained in the main loop() function.  If you do it that way then the other cases would need to reset the range to 0 as the last step within each case #: segment (ie before the break statements;  but not in the case 0: segment).  Then again there may be some rule in the complier that stops the range value from being modified inside the case structure.   This would not be the standard way to do this anyway.   Would be much better to determine the number of button presses, store it in the range variable, and then execute the case statement.   

    Dan,  please create a setup();  a loop(), and a flasha()  which will all be of type void unless they return() a value.       Declare your global variables above the setup() and after the #include file.  

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 13 years ago in reply to billabott

    Hi Billabot,

     

    Yes, the value for range must definitely be set before entering the switch, as the switch depends on the value of range.

    I assumed Dan had posted just a snippet of his code.

     

    Great example in your picture!

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 13 years ago in reply to billabott

    Hi Billabot,

     

    Yes, the value for range must definitely be set before entering the switch, as the switch depends on the value of range.

    I assumed Dan had posted just a snippet of his code.

     

    Great example in your picture!

     

    Cheers,

    -Nico