Arduino
  • Products
  • More
Arduino
Arduino Forum My first switch statement
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 417 subscribers
  • Views 3598 views
  • Users 0 members are here
Related

My first switch statement

e14 Contributor
e14 Contributor over 13 years ago

Im trying to use a switch statement to jump to a different function.  All of the lessons I find just tell me how to turn on leds or outputs.  So I have no idea of what to do here.  So far I have this.

 

 

{

int range;     // I just used this cause it was in an example, I think I need it to name my switch statement. 

int flasha;  //  This is the subroutine I want to run.  I will have more late just trying to figure out the first one.

switch(range);

{

case 0:  //  I don't know why I have  to use "0"  it is just in all of the examples and nothing else works.

state==1, flasha;  // state is my input.  When a button is pressed it will count the number of presses and send it to the approiate subroutine.

break:

}

}

 

When I compile this program I get the error

 

case label '0' not within a switch staetment.

 

Can anyone explain what this means or what I'm doing wrong?

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago +1
    Hey Dan & Nico. Looking at http://www.arduino.cc/en/Tutorial/SwitchCase Would not the range value be determined before entering the switch(range)&case structure? I guess you could set it up that for case…
  • ntewinkel
    ntewinkel over 13 years ago in reply to e14 Contributor +1
    Hi Dan, You are not defining and calling your functions correctly. Remove these two lines, as they define them as integers, which is not the intention: int flasha; int flashb; In the switch statement,…
  • ntewinkel
    ntewinkel over 13 years ago in reply to e14 Contributor +1
    Here's a good link too: http://diyroboticslab.wordpress.com/2009/06/04/ledblink-arduino-program/ It goes into the C programming language, and also has links to what error messages mean.
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Well guys I tried both of you solutions and goot the same result.  And that is the same thing I had before.  It almost acts as if it doesn't even see that line of code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 13 years ago in reply to e14 Contributor

    I only see you changing buttonst in this line:

        buttonst=digitalRead(8);

     

    With that it can only ever be HIGH or LOW, so it won't ever be 10 or more.

     

    If you're trying to increment buttonst with each keypress then you'd have to change your code to detect a button press (debounced so you don't interpret a single press as mutiple presses), and then increment buttonst by just 1.

     

    Also, this code:

    if (buttonst==HIGH)

        {//open state count

      

        if (buttonst==10)buttonst==0;                    RIGHT HERE

     

    you only enter the if... statement if buttonst is "HIGH", which is defined as a single value (probably just 1). Then right after that you check if it's 10. So it will never enter the "right here" statement because it will never be both of those separate values.

     

    Perhaps instead of buttonst you meant to use a separate counting variable like buttonCount ?

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 13 years ago in reply to e14 Contributor

    I only see you changing buttonst in this line:

        buttonst=digitalRead(8);

     

    With that it can only ever be HIGH or LOW, so it won't ever be 10 or more.

     

    If you're trying to increment buttonst with each keypress then you'd have to change your code to detect a button press (debounced so you don't interpret a single press as mutiple presses), and then increment buttonst by just 1.

     

    Also, this code:

    if (buttonst==HIGH)

        {//open state count

      

        if (buttonst==10)buttonst==0;                    RIGHT HERE

     

    you only enter the if... statement if buttonst is "HIGH", which is defined as a single value (probably just 1). Then right after that you check if it's 10. So it will never enter the "right here" statement because it will never be both of those separate values.

     

    Perhaps instead of buttonst you meant to use a separate counting variable like buttonCount ?

     

    Cheers,

    -Nico