Arduino Forum Ethernet board problems
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
  • State Not Answered
  • Replies 9 replies
  • Subscribers 391 subscribers
  • Views 705 views
  • Users 0 members are here
Related

Ethernet board problems

bobcroft
bobcroft over 12 years ago

Hi everybody, I desperately need some help on an ethernet card.  The card in question was purchased from Ebay in the UK.  It is undoubtedly of Chinese origin.  It looks exactly like a genuine Arduino R3 ethernet shield apart from the logo's.  I have tried the ethernet shield attached to several different UNO boards, a genine Arduino UNO, a genuine Arduino R3 UNO and a Freeduino V1.16 which I purchased along with the ethernet card from the same supplier.

 

If I try to load a sketch from the Arduino V1.01 ethernet examples it will load to any of the UNO boards perfectly with no problem, although for the Freeduino you have to select the Duemilanove with 328 instead of UNO board.  When I attach the ethernet board I get the dreaded 'will not sync error'  The sketch compiles but will not load.

A clue was that with the ethernet board attached the LED's on the serial lines did not flash as they do when just loading to the UNO board.  I searched the net and various suggestions included,

bending away the rest pin on the ethernet card - didn't work.

bending away pins 0 and 1 (Tx , Rx) - didn't work.

bending away all the digital and Tx, Rx pins - didn't work.

 

In the end I connected the UNO to the ethernet card with jumpers just pins 5V, Gnd and 10 to 13 inclusive.  With this set up the sketch will load and if I plug the ethernet card into the router there is network activity.  I then loaded the sketch to automatically find an ip address with the DHCP method from the examples library.  It reports DHCP /ip address not found or not obtainable.  Trouble is I do not know if the minimum connections are OK to enable the shield to work properly or if my router is blocking the DHCP request.

 

I would be more confident if I knew why the shield interferes with the sketch upload, and based on my net searches I am not the only person to experience difficulties like the ones described.  I could eliminate the ethernet card issues by possibly buying a genuine Arduino R3 ethernet card but at around £30 in the UK I would prefer not to spend the money at this time.

 

Can someone help please and suggest other things to try or how I can narrow down the cause of the faults further.  I really would appreciate some hel pon this problem

 

Thanks

 

Bob

  • Sign in to reply
  • Cancel
Parents
  • neilk
    0 neilk over 10 years ago

    bobcroft Hi Bob - I've only just seen this - following on from your post re: Arduino Day in Porstsmouth; I live in Sheffield so too far for me as well.

     

    Any way, did you ever solve this?

     

     

    I have a compatible Ethernet shield, also purchased from eBay, and it has worked perfectly from day 1 with both an Arduino genuine R2 and genuine R3

     

    Does yours look like this?

     

    image

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bobcroft
    0 bobcroft over 10 years ago in reply to neilk

    Hi Neil,  actually I live in Bakewell so not too far away from you.  Regarding the Ethernet shield, no I never solved it and yes it did look like the picture you posted.  I bought another couple of shields and they both worked perfectly so I scrapped the faulty one.  It has been a year or two since I posted that enquiry November 2012!

     

    Thanks for asking.

     

    Bob

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • neilk
    0 neilk over 10 years ago in reply to bobcroft

    bobcroft No problem - sorrry I didn't see the post before today!

     

    Do you know of anyone else in our "area" who works with Arduino?

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bobcroft
    0 bobcroft over 10 years ago in reply to neilk

    Neil, no I don't anyone else in our 'area' that works with Arduino although I am sure there must be more than you and I.  In some ways I wish I did because it would be nice to have a get together to share ideas, resolve problems etc.  As well as Arduino I am interested in the ESP8266 radio modules, although they can be a PITA to get working properly.  I have also just bought a Pi2  so I plan to get involved with those too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to bobcroft

    bobcroft,

       For the Pi2 please know that the same card from old Pi will not work unless properly upgraded. Best to plan to rebuild with new card with latest OS.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bobcroft
    0 bobcroft over 10 years ago in reply to clem57

    Clem, thanks for that information, I have never owned a Pi before.  One of my first projects will be to build an internet radio, I have found a brilliant site with loads of information.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bobcroft
    0 bobcroft over 10 years ago in reply to clem57

    Clem, thanks for that information, I have never owned a Pi before.  One of my first projects will be to build an internet radio, I have found a brilliant site with loads of information.