Arduino Forum Self-Destructing arduino code
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
  • State Suggested Answer
  • Replies 29 replies
  • Answers 1 answer
  • Subscribers 406 subscribers
  • Views 3444 views
  • Users 0 members are here
  • self.destructing.arduino.code
Related

Self-Destructing arduino code

dirtdiver
dirtdiver over 12 years ago

Hi everyone,

   so I've been wondering if there is a way to make a hidden button on a device (device wokring with ardunino) that will (once pressed) render the code useless - for example to delete values (val1, val2 ...) or in any way destroy the program that runs that device.

Any ideas?

Thanks,

Lubo (Bo)

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 12 years ago in reply to dirtdiver +2
    Don't patent it! I tell you, it's a waste of time, money and effort. You need to pay thousands of dollars, and here's the worst part: you have to publish a detailed description of your product and how…
  • sonuame
    sonuame over 12 years ago in reply to Former Member +2
    @Rahul,, yeah i am agreed to you , I just told that Reset pin is too much a easy way to stop execution of the microcontroller for that complex machine. sure continously reading the EEPROM values sometimes…
  • ntewinkel
    ntewinkel over 12 years ago in reply to sonuame +2
    I really like Sunil's idea of it only checking after a few days! Much less obvious that way. You might also make it use a jumper on pins instead of a button, to prevent accidental presses. You could probably…
Parents
  • sonuame
    0 sonuame over 12 years ago

    Try connecting one I2C EEPROM 24C256, and write the Encrypted string or Code via arduino board. Lets say 1710 is the code you have written in it.

    Now, Atmega328 microcontroler has one onboard EEPROM, Write a code 1710 in it too...

     

    Now in the Setup Section of your code, Compare any I2C device attached to the uC. and make a female socket for the connection of external EEPROM.

     

    Run your whole program of arduino if and only if the internal EEPROM contains 1710 and dont execute if this code is not saved. Once yopu plug in the EXTERNAL EEPROM, define a logic like, if the code of External and Internal EEPROM matches..it will erase the internal EEPROM completly and hence your entire Arduino

    sketch will be useless. Doesnt matter even if you reset it or Power off...

     

    Hope this one helps...!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to sonuame
    .
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to sonuame
    .