Arduino Forum Self-Destructing arduino code
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
  • State Suggested Answer
  • Replies 29 replies
  • Answers 1 answer
  • Subscribers 406 subscribers
  • Views 3444 views
  • Users 0 members are here
  • self.destructing.arduino.code
Related

Self-Destructing arduino code

dirtdiver
dirtdiver over 12 years ago

Hi everyone,

   so I've been wondering if there is a way to make a hidden button on a device (device wokring with ardunino) that will (once pressed) render the code useless - for example to delete values (val1, val2 ...) or in any way destroy the program that runs that device.

Any ideas?

Thanks,

Lubo (Bo)

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 12 years ago in reply to dirtdiver +2
    Don't patent it! I tell you, it's a waste of time, money and effort. You need to pay thousands of dollars, and here's the worst part: you have to publish a detailed description of your product and how…
  • sonuame
    sonuame over 12 years ago in reply to Former Member +2
    @Rahul,, yeah i am agreed to you , I just told that Reset pin is too much a easy way to stop execution of the microcontroller for that complex machine. sure continously reading the EEPROM values sometimes…
  • ntewinkel
    ntewinkel over 12 years ago in reply to sonuame +2
    I really like Sunil's idea of it only checking after a few days! Much less obvious that way. You might also make it use a jumper on pins instead of a button, to prevent accidental presses. You could probably…
Parents
  • Former Member
    0 Former Member over 12 years ago

    Yeah the EEPROM doesn't change unless you specifically write something else to it. It also stays even when you turn off the power.

     

    The EEPROM on the atmega328p (and most AVRs) is good for around about 100 000 writes. That's probably not going to be a problem for you. The main flash memory of the chip, incidentally, is only good for approximately 10 000 writes. One of my next projects is going to be an "EEPROM destroyer", to see how many cycles I can get out of this thing! Some videos I've seen have gotten about 120 000 writes!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dirtdiver
    0 dirtdiver over 12 years ago in reply to Former Member

    Thanks for all the replies,the EEPROM looks like the thing i need, i will get into it and keep you posted!

    Oh one mroe thing im wokring with a teensy 3.0 with a

    MK20DX128

    32 bit ARM

    Cortex-M4

    48 MHz

     

    and the EEPROM is 2048, i dont know how many writes i have, but it shouldn't be a problem, right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to dirtdiver

    No problems at all! You have 2047 more addresses than you need! Don't worry about how many writes you have either, for your application it doesn't really matter. When you get into data-loggingy stuff then it becomes an issue.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 12 years ago in reply to dirtdiver

    No problems at all! You have 2047 more addresses than you need! Don't worry about how many writes you have either, for your application it doesn't really matter. When you get into data-loggingy stuff then it becomes an issue.