Arduino
  • Products
  • More
Arduino
Arduino Forum My Eyes - LCD Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 416 subscribers
  • Views 360 views
  • Users 0 members are here
Related

My Eyes - LCD Display

e14 Contributor
e14 Contributor over 13 years ago

I always depend on the LCD Display when checking for the status/variables when the firmware is running and usually port2 is dedicated for this purpose. I wonder how will it interface in this new kit if i already have a Shield connected to it. I heard this kit has a debugger but will it be able to see/test for example the position of my finger in the slider or the on/off of the switch?

 

thanks, and by the way this is a cool upgrade kit - arduino shield.

  • Sign in to reply
  • Cancel
Parents
  • element14Dave
    0 element14Dave over 13 years ago

    Hmm perhaps a good question for our arduino group, I will move it over there and see if anyone can give some insight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to element14Dave

    Just be to be clear, what shield/upgrade kit is this?

     

    Some of the shield clashes, can be overcome by changing the pins used.

    They may include a jumper to overcome it, or physical re-wiring might be necessary.

    The pin used are often in the intialisation, or sometime in the .h file that is in the library.

    LiquidCrystal lcd(8, 9, 4, 5, 6, 7); //These are the pins used on this shield (RS, EN, 4x Data pins)

     

    Be warned that only certain pins have certain functions, so random pin selection may not work.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 13 years ago in reply to element14Dave

    Just be to be clear, what shield/upgrade kit is this?

     

    Some of the shield clashes, can be overcome by changing the pins used.

    They may include a jumper to overcome it, or physical re-wiring might be necessary.

    The pin used are often in the intialisation, or sometime in the .h file that is in the library.

    LiquidCrystal lcd(8, 9, 4, 5, 6, 7); //These are the pins used on this shield (RS, EN, 4x Data pins)

     

    Be warned that only certain pins have certain functions, so random pin selection may not work.

     

     

    Mark