Arduino
  • Products
  • More
Arduino
Arduino Forum Reading analog values Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 417 subscribers
  • Views 2438 views
  • Users 0 members are here
  • arduino
  • analog
  • sensor
Related

Reading analog values Arduino

e14 Contributor
e14 Contributor over 13 years ago

Hello everyone,

 

Currently I am working a project..I have 8x8  piezoresistive sensor matrix (i simply used 2 muxs) and I have only 1 analog output that gives me 64 different voltage values (changes depending on the pressure,and its between 2.5 V -5V) for each scan..so what i want to do is,to scan the matrix 10 times and get the averaged values of each cell of the matrix called smoothing..I do know how to do it for single readings but as i mentioned above I get 64 values..so somehow for each loop i have to store 64 values each time and smooth the data..Here what I have wrote..

 


const int numReadings = 64;           // Number of readings for each scan
const int numLoop=10;                   //Number of loops for each scan
float readings[numReadings];         // the readings from the analog input after each scan
float totReadings[numLoop];         //total readings from the analog input  scan
int   index_readings = 0;              // the index of the current reading
int   index_loop=0;                      // the index of the current loop

float average[numReadings];       //Averaged value

int   total[numReadings][numLoop];

 

int inputPin = A0;                     //Determine the pin

void setup()
{
   Serial.begin(9600);                  
  // initialize all the readings
  for (int i = 0; i < numReadings; i++)
  readings[i] = 0; 
  // initialize all the loops
  for(int j=0; j<numLoop;j++)
  totReadings[j]=0;
}
void loop() {
 
  // read from the sensor: 


  totReadings[numLoop]=totReadings[numLoop]+readings[index_readings];

 

  readings[index_readings] = analogRead(inputPin);  //Read the data from sensor (64 values)
 
  // advance to the next position in the array: 
  index_readings = index_readings + 1;

 

  index_loop = index_loop + 1;   
 
  // if we're at the end of the array...
  if (index_readings >= numReadings)             
    // ...wrap around to the beginning:
    index_readings = 0;  
   
  if (index_loop >= numLoop)             
    // ...wrap around to the beginning:
  index_loop = 0;
 
  //Take the average value
  average[numReadings]=totReadings[numLoop]/numLoop;  //Averaged value divided by 10(number of loops)

  Serial.println(average[numReadings]);                              //Print the averaged value 64x1
  delay(100);

 

}
  }
    }

 

image

I havent tested it yet but I do not feel satisfied though..I would be grateful to you if you can give me some ideas for improvement..Thanks a lot in advance..

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago +1
    The ADC is 10 bits of resolution. 2^10=1024. You have thrown away half of your range: 0 to 2.5 volts. Consider doing something to correct that. At some point you will divide by 10 > 8 =2^3. So, the lower…
Parents
  • billabott
    0 billabott over 13 years ago

    The ADC is 10 bits of resolution.  2^10=1024.  You have thrown away half of your range: 0 to 2.5 volts.  Consider doing something to correct that.

     

    At some point you will divide by 10 > 8 =2^3.  So, the lower three bits are of no value any where along the line.  I recommend [0..63]/8 sampled and summed 8 times will produce the average [0..63].    Use a right shift of 3 positions to do the /8 for efficiency.

     

    Since the [0..63] vector must use 16 bit integers you could do [0..63]/8 sampled and summed 16 times then [0..63]/2 will produce the average.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago

    The ADC is 10 bits of resolution.  2^10=1024.  You have thrown away half of your range: 0 to 2.5 volts.  Consider doing something to correct that.

     

    At some point you will divide by 10 > 8 =2^3.  So, the lower three bits are of no value any where along the line.  I recommend [0..63]/8 sampled and summed 8 times will produce the average [0..63].    Use a right shift of 3 positions to do the /8 for efficiency.

     

    Since the [0..63] vector must use 16 bit integers you could do [0..63]/8 sampled and summed 16 times then [0..63]/2 will produce the average.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    Thanks for your informative reply..

     

    Actually output range can be changed depending on the circuit I use so that the output range can be between 0V-5V (eg voltage divider circuit..)..nevertheless,your point was pretty cool,I did not consider it ..So what do you think about the code? are there any points missing? Thanks a lot..

     

    PS:I will add threshold value also..I will not show the output values which are lower than threshold..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    It compiles with Arduino 0023 after removing the two extra } at the end. 

     

    Sorry, I am too tired to read it in depth right now. I would try to stick to integer everything, but that is just me.