Arduino
  • Products
  • More
Arduino
Arduino Forum Linear Pot to control a servo how to adjust the travel of the dial from left to right
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 17 replies
  • Subscribers 419 subscribers
  • Views 2785 views
  • Users 0 members are here
  • linear
  • arduino_uno
  • pot
  • servo_motor_control
Related

Linear Pot to control a servo how to adjust the travel of the dial from left to right

e14 Contributor
e14 Contributor over 13 years ago

Hello....

My supplies:

Arduino UNO

TowerPro Servo

Linear Pot. (radio shack 271-1715 ( http://www.radioshack.com/product/index.jsp?productId=2062354#inTheBox ))

Sketch being used: Arduino / File / Example / Servos / Knob

*******************************************

Ok hope the supplies help you, help me image

 

Everything works wonderful using this example, but my question is:

The lineear pot turns from left to right about, maybe 350°, in laymen terms picture a clock 7 being the start, 5 being the stop.

The servo will turn, when the pot is turned, but it seems as though the servo does NOT star moving until (using the example above until 11, and completes its travels upto 1) sorry for using this as an example, but its the best way to paint the picture.

So can someone tell me what I need to do in order to get the servo to start turning say around 8 and stop right around say 4?

here is the code if you are unfamiliar with it:

// Controlling a servo position using a potentiometer (variable resistor)
// by Michal Rinott <http://people.interaction-ivrea.it/m.rinott>

#include <Servo.h>

Servo myservo;  // create servo object to control a servo

int potpin = 0;  // analog pin used to connect the potentiometer
int val;    // variable to read the value from the analog pin

void setup()
{
  myservo.attach(9);  // attaches the servo on pin 9 to the servo object
}

void loop()
{
  val = analogRead(potpin);            // reads the value of the potentiometer (value between 0 and 1023)
  val = map(val, 0, 1023, 0, 179);     // scale it to use it with the servo (value between 0 and 180)
  myservo.write(val);                  // sets the servo position according to the scaled value
  delay(15);                           // waits for the servo to get there
}

 

Thanks for your help...

Tony

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +1
    Wanna be an EE? Then I recommend you use quadrille paper for the photos next time. That goes for everyone.
  • mcb1
    mcb1 over 13 years ago in reply to billabott +1
    The other option would be to output each of the ADC readings at every hour position. This would then give some figures to set the servo output to. The code is straight from the example on the arduino site…
  • mcb1
    mcb1 over 13 years ago in reply to billabott +1
    Funny while looking at the other servo issue, I had the same idea.... You can specify the max and min pwm values, and this may be a way of overcoming the problem. You'll need to either find someones elses…
Parents
  • billabott
    0 billabott over 13 years ago

    Change

          val = map(val, 0, 1023, 0, 179);

    to

          val = map(val, 0, 1023, 50, 129);

    or

          val = map(val, 0, 1023, 70, 109);


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago

    Change

          val = map(val, 0, 1023, 0, 179);

    to

          val = map(val, 0, 1023, 50, 129);

    or

          val = map(val, 0, 1023, 70, 109);


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    Bill - Hi

    In doing both of your changes, the servo (which is just a 180 degree hobby servo) is not reacting to the contral pot as desired.

    If I may, can you advise me, should I require these in microseconds?

     

    Tony

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    Dear Tony,

       What is the only other possible option?

    change

       val = map(val, 0, 1023, 0, 179);

    to

       val = map(val, 300, 723, 0, 179);

     

    Give it a shot and provide some feedback.  thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    unfortantely its still not working..In a nutshell,...I want to be able to use the entire stroke of the dial;  When its all the way to the left, the servo should be at zero, when I turn it all the way to the right, the servo should be at the 180 degree mark (well 179 actually)  I need to get the pot, very very sensative I guess, in order to make it a smooth ride..I would even be satisfied with about 5 degrees at a time while turn the dial.

     

    Tony

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billabott
    0 billabott over 13 years ago in reply to e14 Contributor

    Terribly sorry, Old Chap.  Have you visited adafruit.com and sparkfun.com for tutorials and other info?  Then there is the official arduino.cc.  They have a wonderful tutorial to be found here: http://playground.arduino.cc/Learning/SingleServoExample  Then there is pololu.com and oomlout.com.  You may even wish to visit letsmakerobots.com.

     

    I am having trouble believing that the potentiometer is linear.  Maybe it is a logrithmic audio pot.

    http://sound.westhost.com/pots.htm

     

    Confirm the following setup: the UNO's analog pin 0 is connected to the wiper of the pot and the low side of the pot is connected to ground AND the high side of the pot is connected to 5 volts.  Use a multimeter to confirm the value of the pot at 12 o'clock is 5K ohm on  both the low and high pins of the pot with respect to the wiper.

     

    Give a full specification of the servo with link to data sheet.  I am willing to bet it is a SG90.  Someone else had one of those and it was nothing but problems.  He had to go buy a normal servo and it then worked fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to billabott

    In response to billabbott from #5 comment:

     

    Hi Bill,

    No believe it, it is a linear pot.  Link to the actual ones purchased: http://www.radioshack.com/product/index.jsp?productId=2062354#inTheBox

     

    The audio’s are: http://www.radioshack.com/product/index.jsp?productId=2062357&filterName=Type&filterValue=Potentiometers

     

    Although they are identical builds, it is my understanding that the audio board is setup differently.  The board on this one is B10K (see pic below) as per the link you provided http://sound.westhost.com/pots.htm

     

    Confirmation of the setup is that the UNO anolog pin is 0 (or A0) and is connected to the center pin on the pot (referred to as 2 Sig in attached pic)

     

    There servo datasheet: is attached as a pdf http://www.kbaam.com/servo/servo.htm

     

    Attached is an actual pic of the servo sitting on my notebook.

    imageimage

    Tony