Arduino
  • Products
  • More
Arduino
Arduino Forum uploading sketch with Windows 7 - no COM3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 418 subscribers
  • Views 564 views
  • Users 0 members are here
Related

uploading sketch with Windows 7 - no COM3

kjhart0133
kjhart0133 over 13 years ago

Hello all,

 

I just migrated all my Arduino stuff to a Windows 7 PC.  I was using a MAC with no problems, but since I've started looking into wireless with XBees I need to use X-CTU which only runs on a PC. <sigh>  X-CTU is necessary to program the XBees in API mode, etc. etc.  Anyway, now I'm having a problem uploading sketches using the PC.  I keep getting the following message:

 

avrdude: stk500_getsync(); not in sync: resp = 0x00

 

I believe this has something to do with the COM port.  I only see COM1 and COM2, which Arduino can't use, COM3 does not seem to come up and the sketches won't upload.

 

Any help is greatly appreciated.

 

Thanks,

 

Kevin H.

  • Sign in to reply
  • Cancel
  • ntewinkel
    0 ntewinkel over 13 years ago

    Hi Kevin,

     

    You need to set up the com port (Mac is soo much easier!).

    Here are the instructions: http://arduino.cc/en/Guide/Windows#toc4

     

    Hope that helps.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to ntewinkel

    Kevin

     

    Some Windows have issues with the UNO.

     

    There were some contributions on the Arduino forums.

    Sometimes there are other windows programs using or monitoring the com ports.

     

    At one stage I resorted to using the Freetronics driver, just to ensure windows loaded a different driver.

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kjhart0133
    0 kjhart0133 over 13 years ago

    Mark and Nico,

     

    Thanks for the helpful information.  I was able to use Nico's instrutions and successfully (I think) loaded the Arduino driver.  I now see COM4 on the list of ports under Tools>Serial Ports.  I still, however, have the same problem even when selecting COM4.  I get the exact same error when I try to upload even a simple sketch like the Blink program:

     

    avrdude: stk500_getsync(): not in sync: resp=0x00

     

    Any other suggestions?

     

    Kevin H.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • terrydark
    0 terrydark over 13 years ago in reply to kjhart0133

    Hi Kevin

     

    Do you have the wireless modules plugged in at the same time you are trying to upload the sketch?  If so, and if the tx/rx lines are connected to the Arduino's tx/rx pins, they may be interfering with the transfer.

     

    Have you tried uploading to a plain vanilla Arduino with no shields or modules?

     

    Regards

     

    Terry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kjhart0133
    0 kjhart0133 over 13 years ago in reply to terrydark

    Terry,

     

    Doh!  That's it!  I have the Wireless XBee shield mounted and neglected to remove the TX/RX jumpers. 

     

    Thanks for the reminder. 

     

    Problem solved!!!

     

    Kevin H.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • terrydark
    0 terrydark over 13 years ago in reply to kjhart0133

    No problem, Kevin

     

    Glad to help

     

    Terry