Arduino
  • Products
  • More
Arduino
Arduino Forum uploading sketch with Windows 7 - no COM3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 418 subscribers
  • Views 567 views
  • Users 0 members are here
Related

uploading sketch with Windows 7 - no COM3

kjhart0133
kjhart0133 over 13 years ago

Hello all,

 

I just migrated all my Arduino stuff to a Windows 7 PC.  I was using a MAC with no problems, but since I've started looking into wireless with XBees I need to use X-CTU which only runs on a PC. <sigh>  X-CTU is necessary to program the XBees in API mode, etc. etc.  Anyway, now I'm having a problem uploading sketches using the PC.  I keep getting the following message:

 

avrdude: stk500_getsync(); not in sync: resp = 0x00

 

I believe this has something to do with the COM port.  I only see COM1 and COM2, which Arduino can't use, COM3 does not seem to come up and the sketches won't upload.

 

Any help is greatly appreciated.

 

Thanks,

 

Kevin H.

  • Sign in to reply
  • Cancel
Parents
  • ntewinkel
    0 ntewinkel over 13 years ago

    Hi Kevin,

     

    You need to set up the com port (Mac is soo much easier!).

    Here are the instructions: http://arduino.cc/en/Guide/Windows#toc4

     

    Hope that helps.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 13 years ago in reply to ntewinkel

    Kevin

     

    Some Windows have issues with the UNO.

     

    There were some contributions on the Arduino forums.

    Sometimes there are other windows programs using or monitoring the com ports.

     

    At one stage I resorted to using the Freetronics driver, just to ensure windows loaded a different driver.

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 13 years ago in reply to ntewinkel

    Kevin

     

    Some Windows have issues with the UNO.

     

    There were some contributions on the Arduino forums.

    Sometimes there are other windows programs using or monitoring the com ports.

     

    At one stage I resorted to using the Freetronics driver, just to ensure windows loaded a different driver.

     

     

     

    Mark