Arduino
  • Products
  • More
Arduino
Arduino Forum Possibility of remote programming Arduino GSM
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 415 subscribers
  • Views 333 views
  • Users 0 members are here
  • remote_programming_arduino
  • bootloader_arduino
  • arduino
Related

Possibility of remote programming Arduino GSM

e14 Contributor
e14 Contributor over 13 years ago

Hello there!

 

I own a Mega 2560 + Ethernet Shield (Wiznet) + Arduino GSM (soon to be bought)

I've been searching around the web and I found Codebender, a web-based bootloader that makes it possible to upload a sketch through the web into Ethernet Shield (compatible with Wiznet). My goal is to do the same with GSM shield, to whenever I want, i would send a sketch over the web and it would be loaded and reprogram the Arduino.

 

Is this feasible? Is this already been done? Will i have to mess with bootloader of Arduino? I'm totally new to this area of programming microcontrollers, but i won't mind learning AVR programming, I just want to make sure I'm not wasting my time. Any guidelines and tutorials pointed out would be great! This or remotely uploading a sketch to SD Card and then flashing new code guidelines will also be welcome!

 

Thanks for any help you can give!

  • Sign in to reply
  • Cancel
Parents
  • Workshopshed
    0 Workshopshed over 13 years ago

    Here's an example that reads the code from an SD Card

     

    http://www.roguerobotics.com/wikidocs/code/bootloader_using_ummc

     

    Here's another that performs a reset via code.

     

    http://www.toptal.com/c/how-i-made-a-fully-functional-arduino-weather-station-for-300

     

    So if you can download a file from the net store it on the card then reset the arduino that will load the new software in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Workshopshed
    0 Workshopshed over 13 years ago

    Here's an example that reads the code from an SD Card

     

    http://www.roguerobotics.com/wikidocs/code/bootloader_using_ummc

     

    Here's another that performs a reset via code.

     

    http://www.toptal.com/c/how-i-made-a-fully-functional-arduino-weather-station-for-300

     

    So if you can download a file from the net store it on the card then reset the arduino that will load the new software in.