Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino I2C display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Answers 1 answer
  • Subscribers 420 subscribers
  • Views 5527 views
  • Users 0 members are here
  • lcd
  • i2c
  • help
  • 20x4
  • arduino
  • module
Related

Arduino I2C display

danyboy
danyboy over 13 years ago

Hello:

I'm a hobbist electronics student and I have been experimenting with arduino for a while. I have worked with character and graphic LCD without any serious problems. I wanted to save wires, so I bought an I2C LCD 20x4 module from ebay. However I have not been able to get it working. I have downloaded the most recent I2C library and I have followed all the instructions but my LCD simply won't work. Instead it lights up like this. The supplier told me that the address of my display is 0x27, but when I use this address nothing happens. After trying different addresses, I dicovered that if I use 0x20 as an address some characters blink randomly with the example code running. the chip on the board is the pcf8574 from Phillips.

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • Workshopshed
    Workshopshed over 13 years ago in reply to billabott +2
    The problem seems to be that pcf8574 is just an I/O expander so it can be wired up differently. The device I chose luckily had a ST7032 LCD controller chip so I did not have that issue but I still had…
  • mcb1
    mcb1 over 13 years ago in reply to danyboy +1
    Daniel You might need to clarify some items here. 1. Your sketch allocates the backlight on D13, but your display is a I2C version and the backlight pins are LCD 16 and 15 (as shown on top left of your…
  • billabott
    billabott over 13 years ago +1 suggested
    #include <Wire.h> #include <LiquidCrystal_I2C.h> LiquidCrystal_I2C lcd2 = LiquidCrystal_I2C(0x27,20,4); // Set the LCD address, # columns and # rows // Create a set of new characters const uint8_t charBitmap…
Parents
  • billabott
    0 billabott over 13 years ago

    Given

    LiquidCrystal_I2C lcd = LiquidCrystal_I2C(0x27,20,4);//  (address of the display, cols, rows)   *

     

    The underlined portion is a function call containing the parameters that define the LCD interface/capabilities.

     

    It compiles for me.  I don't understand how your versions are compiling.   (See Postscript.)

     

    It returns a value into lcd which might be seen by the sketch as a handle;  so that the other library functions can be accessed correctly with the proper parameters.  What if there were two or more LCDs listening on the same I2C wire with different addresses?   Hmmmm?  M'kay!

    for example:

    lcd.print("Hello W.A.T. Bottger");

     

    This is hard stuff, y'all.

     

    Postscript:  Now that the IDE has indexed the existance and location of the library, the original notation also works, but I don't like it as much as the syntactically understandable one on line two of this posting.  Yeah, I know it is a constructor instantiating an object. M'kay.  But who cares?

     

    -=SyntaxMatters=-

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billabott
    0 billabott over 13 years ago

    Given

    LiquidCrystal_I2C lcd = LiquidCrystal_I2C(0x27,20,4);//  (address of the display, cols, rows)   *

     

    The underlined portion is a function call containing the parameters that define the LCD interface/capabilities.

     

    It compiles for me.  I don't understand how your versions are compiling.   (See Postscript.)

     

    It returns a value into lcd which might be seen by the sketch as a handle;  so that the other library functions can be accessed correctly with the proper parameters.  What if there were two or more LCDs listening on the same I2C wire with different addresses?   Hmmmm?  M'kay!

    for example:

    lcd.print("Hello W.A.T. Bottger");

     

    This is hard stuff, y'all.

     

    Postscript:  Now that the IDE has indexed the existance and location of the library, the original notation also works, but I don't like it as much as the syntactically understandable one on line two of this posting.  Yeah, I know it is a constructor instantiating an object. M'kay.  But who cares?

     

    -=SyntaxMatters=-