Arduino
  • Products
  • More
Arduino
Arduino Forum Need Help with Stepper Motor Coding
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 418 subscribers
  • Views 1224 views
  • Users 0 members are here
  • stepper_motor
  • arduino_uno
Related

Need Help with Stepper Motor Coding

e14 Contributor
e14 Contributor over 13 years ago

Hello, I have a NEMA 17 stepper motor with an EasyDriver hooked up to an Arduino Uno. I have a -15 to 15V power supply with 12V powering the EasyDriver. Here is my code and then after the code I will ask my question.

 

int sensorPin = 0;

 

#include <Stepper.h>

 

const int stepsPerRevolution = 200;

 

int dirPin = 8;

 

int stepPin = 9;

 

Stepper myStepper(stepsPerRevolution, dirPin, stepPin);

 

void setup()

{

 

  myStepper.setSpeed(100);

 

  pinMode(dirPin, OUTPUT);

 

  pinMode(stepPin, OUTPUT);

 

  Serial.begin(9600);

}

 

 

void loop()

{

 

  int sensorValue = analogRead(sensorPin);

 

  float voltage = sensorValue * (5.0 / 1023.0);

 

  Serial.println(voltage);

 

  if (voltage > 2.60)

  {

    myStepper.step(100);

   

    delay(1000);

  }

  else if (voltage < 2.40)

  {

    myStepper.step(-100);

 

    delay(1000);

  }

}

 

I have it set at 200 steps per revolution with a speed of 100 RPM. What I want the motor to do is to read the voltage (which it does), turn 180 degrees depending on the voltage, wait one second, and then repeat. With the code I have, it takes three steps, pauses a second, and then repeats. It doesn't go 180 degrees like I want it to do. What can I do to in my code to make it do that?

  • Sign in to reply
  • Cancel

Top Replies

  • colecago
    colecago over 13 years ago +2 verified
    I don't know if you are using library stepper.h correctly. I think the standard Arduino stepper library is for direct driving steppers. Thus Stepper myStepper(stepsPerRevolution, dirPin, stepPin); is meant…
Parents
  • colecago
    0 colecago over 13 years ago

    I don't know if you are using library stepper.h correctly. 

    I think the standard Arduino stepper library is for direct driving steppers.  Thus Stepper myStepper(stepsPerRevolution, dirPin, stepPin); is meant to drive the coils, not controls for step and direction.

     

    Look at this link, it contains an example of something with more of a driver library

    http://www.maxuino.org/stepperdriver

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • colecago
    0 colecago over 13 years ago

    I don't know if you are using library stepper.h correctly. 

    I think the standard Arduino stepper library is for direct driving steppers.  Thus Stepper myStepper(stepsPerRevolution, dirPin, stepPin); is meant to drive the coils, not controls for step and direction.

     

    Look at this link, it contains an example of something with more of a driver library

    http://www.maxuino.org/stepperdriver

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to colecago

    Colecago, just wanted to let you know that you were indeed correct. I went to that link, downloaded that library, and everything is working great! I greatly appreciate your help. Thank you!